STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1442 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 565 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32F4 Problem with USART

Hi, I want to use USART2 as transmitter on stm32f429zi mcu (nucleo board). I configure registers as in the picture, but transmission don't work. I use USART2 on PA2 pin and I need transmission with 115200 baudrate, alternate function is AF7 and usart...

[Debug] Software reset with bootloader

Hello everyone,on my MCU i've loaded a bootloader at address 0x0800000 and a dummy application at 0x0810000, but i'm experiencing some issues on chip reset button on the IDE. At first, when i debug the application no errors are encountered and the ap...

PGior.2 by Associate II
  • 2902 Views
  • 4 replies
  • 0 kudos

Resolved! STM32CubeIDE select target device

Hello,I have 2 NUCLEO boards connected to my computer and I don't see any option to select the target device when I run my project in STM32CubeIDE. I want to be able to run a different program on each board, how can I achieve that ?

Colus by Associate
  • 4169 Views
  • 1 replies
  • 0 kudos

TouchFX on STM32F412G not working

Hi, I am attempting to generate a simple touchgfx project then I generate the code to transfer into an STM32Cubeide project on my STM32F412G Discovery board but every time I do I just get a greyed out screen like attached image is there something I a...

Linkpad by Associate III
  • 1460 Views
  • 1 replies
  • 0 kudos

Resolved! Inquiry about clock activation of stm32cube.

Hello?As the title states, I would like to inquire about the settings of STM32CUBEIDE(V1.13.1) of the STM32F730V8T product.If you select USB_OTG_FS (Dual/OTG, Host Only or Device only) for the relevant MCU, it will be activated in the clock, but USB_...

LSung.1 by Associate III
  • 2769 Views
  • 4 replies
  • 0 kudos

Update USB HOST library in STMcubeIDE

HiI use the USB Host library in some project with STMCUBEIDE , the processor is STM32F779AIYx.The code generator use USB host library 1.0 that have one bug at the line 561 , I must replace this line only time that update my code.I see that there is a...

PZamb.2 by Associate III
  • 2207 Views
  • 2 replies
  • 0 kudos

STM32CubeIDE v1.31.1 error when using 1.17.1 FW patch.

Hi, I have an odd error since updating to 1.17.1 FW on the STM32F7, My setup is :Board -  STM32F769I-DISCOSTM32CubeIDE - 1.13.1After updating with the FW Patch v1.17.1, my project now complains "Code Generation could not be done probably because the ...

SteveFen by Associate
  • 8977 Views
  • 6 replies
  • 1 kudos

hardfault handler

I was using stm32 cube mx to configure a pin to toggle the led so code generated using cube mx and then i just wrote the required function to toggle the led but once the code is compiled it shows zero errrors. when i debugged it and started running t...

pujitha by Associate
  • 1259 Views
  • 1 replies
  • 1 kudos