STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Server problems

 I'm using the NUCLEO-L433RC-P board for the first time. I made a simple code for making a LED blink just to make the card output anything yet I keep getting two error messages. Precisely "Failed to execute MI command: target remote localhost:61234" ...

Mr4 by Associate III
  • 2928 Views
  • 4 replies
  • 0 kudos

Resolved! Flash binaries in STM32F7

Hi all,I have a project on a STM32F7 target and I work on STM32CubeIDE.How can I generate the binaries from the code ? And how can I flash the binaries in the STM32F7 (in NUCLEO-STM32F7ZG board) ?I don't want to use the "flash" button of the app, as ...

Remi99 by Associate II
  • 4091 Views
  • 3 replies
  • 3 kudos

SPI problem in STM32F446 NUCLEO

Hello everyone im currently working on a adc AD7708. I want to read chip from the device but i cant get any valid value. Here is the register sturucture of AD7708:I wrote a basic code to read the chip id from id register. Here is the code:      whil...

mrkayaalp_0-1707326670954.png mrkayaalp_1-1707327149557.png
mrkayaalp by Associate III
  • 6750 Views
  • 19 replies
  • 3 kudos

PA4/SPI_NSS, PA5/SPI1_CLK, PA6/SPI1_MISO

Hi,I have a problem with these pins PA4/SPI_NSS, PA5/SPI1_CLK, PA6/SPI1_MISO I programmed the chip so that those pins are a digital input to check for current present(no current = 0/current present = 1) this process carried out by connecting a wire.a...

rib.1 by Associate II
  • 2308 Views
  • 4 replies
  • 2 kudos

Issue in Input capture for overflow condition.

Good morning community,I am capturing the frequency using waveform generator in STM32.Board: STM32F401RE Nucleo.It is working at underflow condition.Condition is,Reference clock is 25MHz and counter period is 65535. So, minimum frequency is 382Hz and...

MG1 by Associate II
  • 2221 Views
  • 2 replies
  • 0 kudos

Resolved! ST-Link V2 Update Error

I can't update my ST-Link V2When i try to update first it says update error after that update succesfully. 

St link .png
AnilKose by Associate II
  • 2306 Views
  • 2 replies
  • 0 kudos

Resolved! can't make interrup callback work

Hi,I am a newbie to CubeIDE and STM32 Mcus, and have spent hours trying to make interrupt callback work on a Nucleo-STM32G070 board.First, I tried HAL_UART_TxCpltCallback for USART2, this function is not called, then I downloaded an example project T...

Chao_0-1707314144251.png Chao_1-1707314190727.png Chao_2-1707314294871.png Chao_3-1707314348468.png
Chao by Senior II
  • 5407 Views
  • 12 replies
  • 2 kudos

nucleo-h745zi-q is not working

I was using STM32CubeIDE 1.14.1 to write a program to nucleo-h745zi-q and the program I wrote stopped working.I can connect to stm cube programmer.LD5 is also lit.Please help. 

mn0504 by Associate
  • 1318 Views
  • 1 replies
  • 0 kudos

Should ST put Eclipse out to pasture?

Hello,I'm just starting with STM32. Came up with a low-power project, picked a suitable STM32L0 MCU, STLINK-V3PWR to debug and power-profile it, perfect! Then, to my horror, realized that STM32CubeIDE is based on Eclipse. I use Mac with large, high-r...

Zbig by Associate
  • 3562 Views
  • 6 replies
  • 4 kudos

Resolved! B-U585I-IOT02A Undefined reference HAL_I2C

Dear Experts,I'm currently working on a project involving an STM32 board (B-U585I-IOT02A). I would like to use this board as a TCP Server. Therefore, from the STM32CUBEIDE application, I had observed that there is an example project in which it is po...

Nicolas_G_0-1707315922146.png Nicolas_G_2-1707315922156.png Nicolas_G_6-1707315969626.png Nicolas_G_3-1707315922158.png
Nicolas_G by Associate II
  • 2382 Views
  • 2 replies
  • 3 kudos