STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

how to solve semaphore issues: button toggling issue

/* USER CODE END Header_Normal_init */void Normal_init(void const * argument){  /* USER CODE BEGIN 5 */  /* Infinite loop */  for(;;)  {//while(HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_13)); char *msg1 =  "hello mid\r\n";HAL_UART_Transmit(&huart3, (uint8_t *...

Akshay_ by Associate II
  • 1360 Views
  • 1 replies
  • 0 kudos

Application code slower in 1.14.1 vs 1.5.0

Hi all!I have been working on a C++ project for the STM32F476G-DISCO, which was originally created in 1.5.0 of the IDE. Given the QoL improvements in the IDE updates, I thought it would be worth updating.My application has image processing included s...

JaredP by Associate
  • 1603 Views
  • 2 replies
  • 3 kudos

Resolved! I tried to add a string to a text file saved in "microSD" using "f_write" of "FATFS", but the writte

 Hello everyone in the community.■What you are having trouble with :→I tried to add a string to a text file saved in "microSD" using "f_write" of "FATFS", but the written content was not saved.■Specific phenomenon:→As shown in the PG below, the resul...

toka_0-1707194525671.png
t-oka by Associate III
  • 2431 Views
  • 2 replies
  • 0 kudos

'No ST-LINK detected' in MacOS STM32CubeIDE using M3 chip

Hi,I am using an STM32H755 and have it connected to a MacOS with an M3 chip, utilizing STM32CubeIDE with ST-LINK installed. The code successfully builds, but when I attempt to transfer the code to the board by clicking the 'run' icon, I encounter the...

No completions available for HAL function

Hi,I try to use HAL_ADC_ConvCpltCallback function under user code begin4, but it does not autocompleted under that section. On the contrary, it is auto completed under USER BEGIN2.Could you please point me to the right direction ?   

demir_0-1707246352683.png demir_1-1707246565285.png
demir by Senior II
  • 1396 Views
  • 1 replies
  • 1 kudos