STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1433 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE on Windows Server 2019 for all users?

I have installed STM32CubeIDE + TouchGFX on a Windows 2019 server.It works for my account, but it does not work for other users.Question: Is it possible to install STM32CubeIDE for all users? I mean that other uses do not need to reinstall the softwa...

awiernie by Senior II
  • 934 Views
  • 0 replies
  • 0 kudos

cube-mx, xcube-ai, stm32h7 model generation.

Hello,Xcube-AI model generation. input file tflite.During model generation(Analise) i am getting error with Analyzing modelC:/Users/Yashwanth.LAPTOP-5EKATUMV/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/8.1.0/Utilities/windows/stm32ai anal...

Resolved! STM32CubeIDE build analyzer problem

Hi folks, I use latest STM32CubeIDE on Linux and noticed that build analyzer always updates "Memory Regions" tab for previous build configuration (whatever it was Debug or Release).No matter how many times I rebuild code in "Debug" configuration, the...

Lex by Associate III
  • 8325 Views
  • 3 replies
  • 0 kudos

USART3 Receive interrupts issue.

Hi, I'm using the USART3 on interrupt mode with the STM32F407 chip and I cant figure out why the recive function is not working.I'm transmiting from a STM32F7 a buffer like this: "$en:X# to the F4 but this buffer never arrives when debugging. I'm sur...

ferdlf by Associate III
  • 5646 Views
  • 7 replies
  • 1 kudos

Resolved! Headlessbuild error when using cmd to build project

When is use those command to compile my project, some error occurred,However,  When I use gui to build the same project, the result is ok. command:./stm32cubeidec.exe --launcher.suppressErrors -nosplash -data D:\Workspace\Firmware -application org.ec...

Nico4 by Associate
  • 2630 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CureIDE can not surpress warnings

I integrated one open source software module into my project, but I found that there are a lot of warning about unused functions, so I tried to surpress that by adding "-Wunused-function" in CubeIDE, and found the configuration is correct by checking...

HXiao.1 by Associate II
  • 1494 Views
  • 2 replies
  • 1 kudos

import mdk-arm to stm32cudeide

I start the project(SDIO+FATFS)from the .ioc file and also regenerate the project from CubeMX with IDE as a toolchain and unchecking the "Generate under root". But after i generated, the project does not have anything. 

Jacob3104_0-1710902505836.png Jacob3104_1-1710902559570.png

post build

Dear Sir.I have designed a bootloader that stat from 0x8100000 , length of 40k bytes,there is also a signature of 2 bytes 0x23,0x45, at @ 0x80f6000,at last the runtime code that start from 0x8100000.Is it possible to use STM32IDE's post build to make...