STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1508 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 573 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

import mdk-arm to stm32cudeide

I start the project(SDIO+FATFS)from the .ioc file and also regenerate the project from CubeMX with IDE as a toolchain and unchecking the "Generate under root". But after i generated, the project does not have anything. 

Jacob3104_0-1710902505836.png Jacob3104_1-1710902559570.png

post build

Dear Sir.I have designed a bootloader that stat from 0x8100000 , length of 40k bytes,there is also a signature of 2 bytes 0x23,0x45, at @ 0x80f6000,at last the runtime code that start from 0x8100000.Is it possible to use STM32IDE's post build to make...

Errors galore after updating STM32CubeIDE

I updated to the STM32CubeIDE 1.15 WIN, and since then my project has thrown up 100+ errors. It doesn't recognise "u_char" or "uint" or "caddr_t".  It throws up error "expected ')' before 'GPIO_TypeDef'" in the below statement : void Write_MFRC522(u_...

How to debug print with Nucleo L476RG board with st-link. I use printMsg command , it compiles Ok, but no output on itm window. I am using stm32cubemxide 1.01 to do this. Regards, Ronald.

I've made my own lab.it is 4 switches on gpio input's with interruptit switches 4 leds, so i you press switch 1 , led1 goes on , it works fine.But i want to see debug messages in ITM terminal screen and i don't het this up and running.hopefully some...

RHofm by Associate II
  • 3174 Views
  • 2 replies
  • 0 kudos

Resolved! Installing X-CUBE-TCPP v4.0.0 in STM32CubeIDE

I have installed the example USB-C projects using the General/Import Projects from Folder or Archive option targeting the NUCELO-G474RE:DRP1M1_DRPSNK1M1_SinkSNK1M1_SourceWhat do I need to do to make these regular STM32 projects such that the Build Al...

alw by Senior
  • 2503 Views
  • 2 replies
  • 0 kudos

live expression is not opening

Hey ST, I was using cube IDE, after selecting  MCU board, we need to give project name,  while in targeted project type name i kept at  empty,  as i don't want to use IOC configuration. After successfully  writing  and debugging the code ,  if I am  ...

Sushmita by Associate II
  • 3872 Views
  • 7 replies
  • 0 kudos

Resolved! Delayed in PWM and interrupt

HiI'm implemented the most simple pwm generation and using interruptions in F401RE with TIM1. But a delay has been in the PWM generation and the update event interrupt (underflow and overflow) the most large pulse is the PWM and the another the when ...