STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 561 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Not able to flash stm32g030c8t6 with st link v2

-------------------------------------------------------------------STM32CubeProgrammer v2.16.0-------------------------------------------------------------------   Log output file: C:\Users\adity\AppData\Local\Temp\STM32CubeProgrammer_a09404.logST-LI...

Resolved! How to open "Live expressions" tab?

I have accidentally closed this tab (with X) so it no longer shows in my debug tabs, and can't find where is the setting to re-add it :(I'm using Cube version 1.10.1

"stm32cubeidec -build all" results to extra build runs

I have tried to build an example STM32H7Cube project with a command line script (attached) and got that the each CM7 and CM4 project configuration is built twice: the "Release" for CM7 is built twice, then the "Debug" for CM7 is built twice, and then...

ERROR by Senior
  • 925 Views
  • 0 replies
  • 1 kudos

Resolved! TIM2 as a sequencer for TIM5, TIM1 and TIM8

Part: STM32L4R5ZIT6I would like to use TIM2 to increment 3 other timers at different times:TIM2 is incrementing from an external clock and rolling over at a set period.1. TIM2 rollover would increment TIM52. TIM2 Compare 1 would increment TIM13. TIM2...

RChap.1 by Associate III
  • 3147 Views
  • 5 replies
  • 0 kudos

Resolved! Cube IDE 1.15.1 Freeze when creating example project

Hi, I am trying to create an example project for my NUCLEO-F401RE board by following the following steps:1. Completely clean Debian 11.9.0 installation (in virtual machine)2. Download and install STM32CubeIDE 1.15.1 (STM32CubeIDE-DEB)3. Launch the ID...

FJons.1 by Associate II
  • 6132 Views
  • 8 replies
  • 0 kudos

Resolved! Installation of SonarLint fails

When I try to install SonarLint from Eclipsemarkete place I get the following errorUnable to read repository at https://eclipse-uc.sonarlint.org/content.xml. Certificate chain is not validSTM32cubeIDE 1.7.0 on WindowsI asked the question on the Sonar...

Stefan1 by Associate III
  • 3362 Views
  • 3 replies
  • 0 kudos