STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1403 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Could not download IDE

Hello I am currently logged in to st.com and attempted the download but failed.It did not show any sign of error, but it keeps going back to initial page.Is there any issue with the download now?I am attempting on windows 11 pro 22631 build via lates...

godSSom by Associate
  • 1015 Views
  • 1 replies
  • 0 kudos

Resolved! HW or SW issue?

Hallo,I needed more performance for my project, so I replaced my STM32F401 Blackpill by a WeAct STM32H723VGT6 board. I adapted my HW to accomodate the different layout of the H723 board and modified my application where needed because differences in ...

DebugError_H723VGT6_20240508.png
FredS by Senior
  • 13321 Views
  • 15 replies
  • 3 kudos

stm32 ide download problem

Hi         I am new to stm32 and try my stm board via arduino ide bcoz when ever I try to download the software a message is shown as belowthis software is not available for download. regards.

ap2miz by Associate
  • 1155 Views
  • 1 replies
  • 0 kudos

Resolved! starting two PWM timers with a defined offset between each other

Hi,I want to start two PWM timers at the same frequency but with an offset of a few 100 us to few ms range but it doesn't appear to work. I've been experimenting with something like this:PCLK1Freq = HAL_RCC_GetPCLK1Freq()*2; TIM3->ARR = (uint32_t)(((...

debug by Associate III
  • 1547 Views
  • 1 replies
  • 1 kudos

Could not determine GDB version

I am receiving this message 3 out of 4 times (approximately) after I just "upgraded" the IDE to 1.15.1 while using a Nucleo STM32H563 board. My debugger config screen looks like 

Capture.PNG Capture2.PNG

i2c clock stretching

Hi,now I'm implementing i2c with 1 master(U575ZI-Q) and 3 slave(L432KC) boards. master transmit dataBuf to slave HAL_I2C_Master_Transmit_IT(&hi2c1, addr<<1, dataBuf, sizeof(dataBuf)); and Slave receive it.HAL_I2C_Slave_Receive_IT(&hi2c1, dataBuf, siz...

eunni_0-1715233400867.png
eunni by Associate III
  • 2842 Views
  • 3 replies
  • 0 kudos

DCMI D1 waveform not showing

I'm trying to get image data through DCMI using ov2640, but other pins' signals come out well, but D0's signals don't show waveformsHardware connectivity is no problem. Is there anything I should pay attention to in software or clock?

achovy by Associate II
  • 1385 Views
  • 1 replies
  • 0 kudos

Resolved! ADC Triggered by Timer

Hello community , Am using STM32H745ZIT6 MCU in that  configured ADC (4 channnels)  triggered by timer and data collected in DMA .ADC is tiggered by timer (all the 4 channels at a time ) . I want to trigger each channels seperately(in a single ADC) b...

SA  V.1 by Senior
  • 1555 Views
  • 1 replies
  • 0 kudos

Cube IDE Version: 1.15.1 Problems

I am using Mac Os I installed Cube IDE Version: 1.15.1. And tried to progarm ,i lost a lot of time by software error.When i configure the .ioc where I configured TIM1 with some parameter .After the  code generated and wrote some programs ,but not wor...