User Activity

Hi All,I have created a copy of an existing CubeIDE project "riverdi-70-stm32h7-lvgl" as you see below. The second project doesn't have the active CM7 project feature that allows to build, it just shows CM7 folder. What is the reason for this? I trie...
Hi all,Is it possible to capture image from an IP camera which is connected to an STM32 MCU via ethernet port? An external RAM can be added to handle the data traffic. Due to multiple reasons I cannot use a digital camera instead of an IP camera.Does...
Hi,I have a custom board with STM32f427VG and KSZ8041NL PHY. My ethernet communication is working well in STMCube IDE 1.8.0. But when I try to configure ethernet in ver:1.9.0 I don't see a input box for PHY address. It says it some ethernet settings ...
Hi all,I am working on a project that transmits UDP packet to a remote IP and port. I need to receive a broadcast packet from a particular source port. Below is my current UDP initialization.I am using LWIP stack for UDP communication. How should I i...
Hello,I am configuring KSZ8863 3 port switch over I2C. And the slave address Read/Write address is oxBF/0xBE respectively. In the HAL reference manual it says the address should be shifted left before calling the interface. It's confusing, if I am sh...
Kudos from