STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Using stack-protector with CubeIDE

I'm looking for some info about and help with using -fstack-protector and similar compiler options with STM32CubeIde. I've never used these flags before, but enabling them does seem to compile fine. Am I correct in assuming that the GCC supplied with...

Konami by Senior II
  • 3735 Views
  • 2 replies
  • 0 kudos

ST Cube IDE 1.15.1 - Launch Group/Debug Issue

Hello to everyone,for my graphical application I usually use custom boards with STM32H750XB mcu.For all my projects I always used STMCube IDE 1.6.1.Code is executed from external qspi flash, so I create a bootloader to launch the application and debu...

afici by Associate II
  • 2205 Views
  • 2 replies
  • 0 kudos

Resolved! Uint16_t Build Errors within STM32CubeIDE 12.1

Hey ST Community, I started getting errors within STM32CubeIDE, throughout all workbenches randomly, after working on a new project.The errors involve uint16_t,  such as:-'error: unknown type name "uint16_t''-"error: unknown type name 'uint16_t'; did...

AEng7 by Senior
  • 9368 Views
  • 7 replies
  • 2 kudos

Resolved! EEPROM (M24M01E-F) Page accessing

Hi,For my project, I am using an M24M01E-F I2C EEPROM. My application requires writing and reading data page-wise. According to the datasheet, the EEPROM has a capacity of 1 Mbit (128 KB). I need clarification on how many pages I can able  write to u...

Rishvana by Associate II
  • 4048 Views
  • 8 replies
  • 3 kudos

Please change GCC stack canary to be weak

Hi Could you please change the library implementations so that  void __stack_chk_fail(void)andunsigned long __stack_chk_guardare defined as weak?I have tested it with GCC 11.3.rel1 and 12.3.rel1 and on both i get "multiple definitions of __stack_chk_...