STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1427 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! (M24M01E-F) Data storage

Hi,For my project, I am using an M24M01E-F I2C EEPROM. In this application need to store sensors offset values (float data type) in EEPROM. whether it can be able to write/ read float value. Regards,Rishvana M

Rishvana by Associate II
  • 1479 Views
  • 2 replies
  • 1 kudos

Broken server install / Debian 12.5 Bookworm

Hi,Recently, when I tried to install the Debian Linux version of STM32CubeF4 on my Debian Linux (v12.5) Bookworm system, I began by trying to install a package that included Server 2 in its name. The server install hung at 50% installed. Each time I ...

How can I change the build analyzer color preferences?

I use the dark theme of the IDE and can find no preference settings to change the colors for the build analyzer output. The IDE shows the usage info with light gray text on a bright green background which (to my eyes) is almost unreadable. I say almo...

Build Analyzer Color Preferences.PNG
DSudo.2 by Associate III
  • 1403 Views
  • 1 replies
  • 0 kudos

Convenience of CubeIDE

It is done incorrectly that after pressing the "Debug" button while the project is being compiled and loaded into the MCU - it remains possible to press the "Debug" button again, which is incorrect (this will corrupt the normal course of the process)...

OlegAjax_0-1723713520475.png
OlegAjax by Associate II
  • 1109 Views
  • 1 replies
  • 0 kudos

CubeIDE - debugging startup process

When I start debugging - there is unnecessary focus switching between the startup_stm32f* editor, the focus is constantly broken from the current window and CubeIDE switches the focus to itself - this is strange behavior. Is it possible to remove the...

OlegAjax_0-1723714218174.png
OlegAjax by Associate II
  • 1150 Views
  • 1 replies
  • 0 kudos

Resolved! PWM configuration

Hi, I'm a newbie in this embedded board and I'm having a hard time setting up the PWM pins. I'm currently using an STM32F103RB with a bldc motor driver shield that has pin 5, 6, 9 for PWM input.The corresponding pins for them are PB4, PB10, PC7 so I ...

Issue: No source available for Bootloader

Hello,My project was working fine, but suddenly I cannot debug or run it with the original bootloader anymore. The project is created and generated by TouchGFX Designer.This is the error message I get when I try to debug/run the project.I am sure tha...

mids400_0-1723200878741.png
mids400 by Associate III
  • 2718 Views
  • 4 replies
  • 1 kudos

DS18B20 not registering with internal pullup resistor

I am trying to use the DS18B20 temp sensor on a stm32h7 board to display the current temperature using putty, and if the temp is higher than 45 degrees celsius to display a heat warning, but for whatever reason the sensor is not beign registered. I h...

smakivic by Associate
  • 2162 Views
  • 3 replies
  • 1 kudos

Is there a software update override option?

Hello,I am a Lab Instructor at the University of Waterloo, Ontario Canada.I am using the STM32CubeIDE tools in my lab. There are about 200 students using my lab every term. I have the STM32CubeIDE tools running on 24 workstations in the lab and I hav...

CPope.2 by Associate
  • 2832 Views
  • 3 replies
  • 2 kudos