STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 564 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

files not being recognized if inside folder

I will attach my project below if you want the code for reference.         I am making a HMI for construction workers for reference. Although my screen does everything I've needed thus far it has been hard to organize my code because I keep running i...

tmehok by Associate III
  • 2030 Views
  • 3 replies
  • 0 kudos

Resolved! .ioc file doesnt open

Hi everyone, Actually, the subject line describes my problem completely. I tried to improve my IOC file yesterday with debugging, checked it again this morning, and it was working perfectly. But now, after an update or something similar, it suddenly ...

hannah by Associate II
  • 10694 Views
  • 11 replies
  • 1 kudos

Resolved! <string> not found when included in a .h file

Hi,I need to use <string> (standard in C++ libraries and am working in a C++ project. My header file is a normal .h, and on compiling I get the below. Oddly, if I select string in the header and view declaration, the standard file opens up just fine?...

mtechmatt_0-1725368189958.png
mtechmatt by Associate III
  • 1638 Views
  • 1 replies
  • 1 kudos

Resolved! STM32F103 FreeRTOS CMSIS V2 issue

Hello,A project generated using FreeRTOS CMSIS V1 compiles and works, but the same project using CMSIS V2 does not compile.freertos_mpool.h is missing while it is present in projects using the F4 family.It looks that this old issue has been solved fo...

zeboss49 by Associate III
  • 3626 Views
  • 2 replies
  • 0 kudos

Resolved! Support for STM32H757

When trying to generate code using STMCubeMX, both TrueStudio (understandable) and STM32CubeMXIde are greyed out. I have the newest version of CubeMX, CubeMXIde, and TrueStudio installed.When will the 757 be supported? We are in a rush in developin...

RGari by Associate III
  • 1424 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeIDE not flashing my board anymore

Hello everyone,I'm currently facing an issue with STM32CubeIDE when trying to flash our board.It wasn't like this before and nothing special really change in the project configuration but now when I try to run the code I get this : STMicroelectronics...

Pkemarco by Associate III
  • 4627 Views
  • 8 replies
  • 0 kudos

Resolved! UART Data Transmission on STM32H755 Nucleo Board

Hello everyone,I'm reaching out in hopes of getting some urgent assistance with a project I'm working on for my studies. The deadline is approaching quickly, and I need to resolve this issue as soon as possible.Project Overview:I'm developing an anom...

Student1 by Associate II
  • 8420 Views
  • 11 replies
  • 9 kudos

Resolved! USBD_LL_PrepareReceive stops filling buffer content

I'm making a simple USB MIDI implementation, and using a DAW to send note-on/note-off events from the computer to the device. The maximum packet size is 64 bytes, events are 4 bytes each so up to 16 events should fit in one packet.When I send one or ...

Selection_132.png
iforce2d by Associate III
  • 1317 Views
  • 1 replies
  • 0 kudos

Resolved! IDE not generating .elf file while importing project

Dear,I am facing a problem while importing a project (that is built from another computer) to a new system, IDE is not generating .elf in the debug folder. While compiling is also warning about the same. Suppose I take a .elf from the old system and ...