STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1534 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 586 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! M7 core works but not M4

good morning, I began today on a nucleo 144 and so discovered the double core.so I wanted to make each core work independently, and used a led blinking code. unfortunately, it only works on core M7 and not on core M4. I do not know why, maybe I misun...

Jad by Senior
  • 1199 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE 1.14.0 -> old issue

Hellothe brand new 1.14.0 has the same issue like the older one.an unnecessary file is opened after the 2nd debug session.It's annoying that STM can't get this solved.padawan 

padawan_0-1700729625642.png
padawan by Senior II
  • 7332 Views
  • 9 replies
  • 12 kudos

Debugging STM32F429 on Disco board with CubeIDE

I am using the STM32F429I-DISC1 board and flashed code to the board using the STMCUBEIDE but when i am debugging i have encountered this error(attached the image). I have also tried the external loader file M29W128GL_STM32f4x9I-EVAL and also the fla...

Muthamizh_0-1726114488711.png
Muthamizh by Associate II
  • 2728 Views
  • 4 replies
  • 0 kudos

Cube IDE 1.16.0 and STlink v3 - cannot find debugger

This sort of thing is a way of life with these ST tools (been using Cube IDE for 6 years on this project) but this one I am unable to fix. Is there some special setting needed under Debug (under project/properties)?   STMicroelectronics ST-LINK GDB s...

PHolt1_0-1721987017824.png PHolt1_1-1721987204042.png
PHolt.1 by Senior III
  • 13361 Views
  • 28 replies
  • 4 kudos

Resolved! Debugging Issues STM32F429I

 I HAVE USED THE ST LOADER  YOU HAVE SUGGESTED FOR MY LAST PROBLEM AND NOW ALSO IT REPEATES TEH SAME PROBLEM THERE IS PROBLEM WHILE OPENING THE STM32_PROGRAMMER_CLI.EXE. SUGGEST ME A SOLUTION FOR THIS OR AN ALTERNATIVE. THIS IS THE DEBUGGER CONFIGURA...

Muthamizh_0-1725860329559.png Muthamizh_1-1725860589082.png
Muthamizh by Associate II
  • 5784 Views
  • 12 replies
  • 1 kudos

Resolved! STM32CubeIDE Project For Static Library

I had a STM32CubeIDE v1.15.1 static library project against which I was linking with no problems. The static library project created the lib*.a file fine.After moving the project to a different workspace, the lib*.a file is no longer created. Instead...