cancel
Showing results for 
Search instead for 
Did you mean: 

Assign a variable to the c-file line number.

Mike xx
Associate III

I have a FreeRTOS queue with many calls from various tasks.

I would like to assign elements of a variable that is passed into the queue with the file name and line number of the task that is placing the variable on the queue.

I have a corruption issue that might be a stack or perhaps an array that is being sent to the queue that is not copied but sent as a reference?

At the moment I have started to hand code the line numbers, but it's not ideal.

Can anyone help?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Andrew Neil
Super User

__FILE__ and __LINE__

 

https://gcc.gnu.org/onlinedocs/cpp/Standard-Predefined-Macros.html

 

EDIT:

GCC also provides __FILE_NAME__ to give just the name, without path:

https://gcc.gnu.org/onlinedocs/cpp/Common-Predefined-Macros.html

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

View solution in original post

3 REPLIES 3
Andrew Neil
Super User

__FILE__ and __LINE__

 

https://gcc.gnu.org/onlinedocs/cpp/Standard-Predefined-Macros.html

 

EDIT:

GCC also provides __FILE_NAME__ to give just the name, without path:

https://gcc.gnu.org/onlinedocs/cpp/Common-Predefined-Macros.html

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Mike xx
Associate III

Many thanks for the quick reply.

My previous google searched had failed me. I hadn't search with gnu or gcc.

I thought they must exist as they do for the IAR compiler.

You're welcome.

Yes, they are part of the C Standard - apart from __FILE_NAME__

If that's answered the question, please mark the solution.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.