STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1548 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Program size calculation using STM32CubeIDE

 Hi, When compiling program using Keil IDE, understand that the program size that flash to MCU can be calculate by:Program size = Code + RO + RWHowever, when compiling using STM32CubeIDE, how to know the program size going to flash into the MCU flash...

chai2145_1-1728379506281.png

Error: Code generation could not be done because the necessary firmware package is missing. Not able to complete STM32Cube project creation.

I hope this is the right thread for my question. I recently decided to switch to STM32CubeIDE from the online compiler as there is debugging and is offline capable.I downloaded STM32CubeIDE and went to create a new STM32 Project. I selected my dev bo...

0693W000006F5mEQAS.png 0693W000006F5n2QAC.png 0693W000006F5nqQAC.png
CWill.3 by Associate II
  • 16095 Views
  • 18 replies
  • 1 kudos

CubeIDE Memory view - why different fonts?

Why am I getting 2 different fonts in these Memory views?If I now create a new view, it uses a different font: It seems that it only happens in a newly-created view; if I switch from that last one to one of the earlier views, then switch back again, ...

AndrewNeil_0-1728052642767.png AndrewNeil_1-1728052675908.png AndrewNeil_2-1728052764836.png AndrewNeil_3-1728052915084.png

Resolved! STM32IDE cannot sometimes find an included linker file

I have a complex project that has multiple sub-projects inside. One of these projects has an additional .ld file called "STM32L431KCUX_SHARED.ld". This file is a linked resource in other sub-projects and normally it works without an issue, every "STM...

MO94 by Associate III
  • 4653 Views
  • 4 replies
  • 1 kudos