STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1547 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

HOWTO: Saving versions of a project using git

I had an issue, that i could not reproduce, because i could not restore the exact state of the project. The CubeIDE has its own version control for each file, which is of no great use, since the project consists of many files. Because of that i devel...

Tobe by Senior III
  • 2171 Views
  • 0 replies
  • 0 kudos

Resolved! CubeMX behavior when open from CubeIde.

Hi all!,I notice a different behavior from CubeMX, when starts alone or is called from CubeIDE.When I open CubeMX without CubeIDE, it works as espected. But when CubeMX is open from CubeIDE, it works in a strange way. Per exemple, when I try to put a...

JAlca_0-1730536844987.png JAlca_1-1730536935702.png JAlca_2-1730537000276.png JAlca_3-1730537019658.png
JAlca by Senior
  • 1975 Views
  • 3 replies
  • 1 kudos

stm32cubeIDE project configuration using CLI

Hi. I'm aware that there's a cli tool called  STM32CubeCLT which is used for building programs for stm32 MCUs. But, is there any way that we can ask stm32cubeIDE to perform the following steps?install/remove a certain cmsis-packconfigure a certain pr...

Resolved! Stm32h753i-eval2 USB Host FS

Hi, I need help generating an .IOC file through the cube generator. What I need is USB Host FS. I'm having trouble getting it to work, specifically, there's no voltage on the VBUS output.I want to mention that I was able to create a USB Host HS that ...

ikogman by Associate II
  • 6738 Views
  • 10 replies
  • 3 kudos

Resolved! Update CubeIDE fails missing public key

Updating the cubeide generates this error:An error occurred while collecting items to be installedsession context was:(profile=STM32CubeIDE, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).Result of processing steps.OK...

j1s1e1 by Associate
  • 8734 Views
  • 9 replies
  • 5 kudos