2024-06-12 02:34 AM
Hello,
I will debug a application on the STM32G030F6 which are use to 90% the low poer sleep mode. For this I will show the changes of variables in RAM and Flash also the changes of SFR from the MCU hardware like SPI in real time. I will also manipulate variables in the RAM.
Now I see in the "Live Expression" view frosen values. The changes of the values are verry short.
How can I change the update period of the SFR and "Live Expression" view?
Thanks for our help,
Bernd