User Activity

Am using 1.16.0.This picture tells the whole story:Am I doing something wrong or is Live Expressions broken?
Hello,According to the manual , "This attribute, attached to a variable with static storage, means that the variable must be emitted even if it appears that the variable is not referenced."In the following code, unreferenced_variable is always discar...
Hello,I'd like to create an output section called .cal_data capturing constants from a particular object file called const_params.o so I have created the following additional linker script entry based on the GNU syntax: .cal_data : { const_par...