STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1433 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32U5G9VJT6Q not supported?

Hi,I just tried selecting the STM32U5G9VJT6Q in CubeIDE and the "Next" button to start a project based on it is not enabled and there is a note at the top of the window saying it is not supported (see attached screenshot)?I assume that is incorrect a...

Amz 001530.jpg
Ricko by Senior III
  • 1697 Views
  • 2 replies
  • 2 kudos

STM32CubeIDE for Ubuntu 24.04

Hello All,     I am using Ubuntu 24.04 and STM32 Cube IDE 1.16 version. When I try to  burn code to a STM32F401RE Nucleo board. I am getting below error. Could not determine GDB version using command: arm-none-eabi-gdb --version arm-none-eabi-gdb: er...

NNada.1 by Associate II
  • 3212 Views
  • 2 replies
  • 0 kudos

Resolved! CubeIDE gets stuck launching Debug

I'm trying to debug a STM32 project on an STM32 IoT Discovery Node Board (B-L475E-IOT01A1) from my MacBook Pro (M1 Max running Sonoma 14.5). Every time I build and start a debug session, the process gets stuck on "Launching : Performing pre-launch ch...

Screenshot 2024-10-06 at 23.14.59.png Screenshot 2024-10-06 at 23.14.47.png
klaytonme by Associate II
  • 3118 Views
  • 4 replies
  • 0 kudos

Resolved! Compare TrueStudio with STM32CubeIDE

I'm using TrueStudio for my previous product coding/debugging.  I downloaded some example projects from ST website,  there are options for IAR/Keil/STM32CubeIDE, is TrueStudio fully replaced by STM32CubeIDE?I'm get used to TrueStudio, is STM32CubeIDE...

Messed-up source path

Hello Community!In my current project with the NUCLEO-H7S3L8, I am encountering some problems that seem a bit confusing and strange. As a starting point i used this Template from Github, which was the only way i didn't receive an error during program...

R_Zip_1-1730115473737.png R_Zip_0-1730115408890.png
R_Zip by Associate
  • 882 Views
  • 0 replies
  • 0 kudos

Resolved! Unable to select PB6 for I2C1_SCL on STM32F103C8

Hi,Trying to use I2C1 with REMAP=0 and as long as understand the SCL and SDA pins are PB6 and PB6. Along with I2C I am using some other peripherals as well. I am unable to select PB6 for I2C SCL PIN. Please see attached screenshot. Not sure why it wo...

technofection_0-1729854964045.png