STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1103 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 478 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! CubeIDE Resume (F8) button active when it shouldn't be

Hello,I am facing a small but very boring issue with the Resume (F8) button of the top tool bar.This button is active when it should not be, while download is in progress and if you click on it, the download fails.This behavior is systematic.Randomly...

zeboss49 by Associate III
  • 1504 Views
  • 2 replies
  • 0 kudos

Resolved! M1 Macbook pro can't use st-link to run programs

Hello. The following is machine-translated so it might seem a bit strange. I'd like to ask if I can use my only computer, the "MacBook Pro with M1 version", to connect to ST-LINK V2 to program the STM32 on a C8T6 chip's PCB board. I've tried using V1...

yangyan by Associate III
  • 12776 Views
  • 19 replies
  • 3 kudos

Resolved! Strange logic problem after compilation in CUBE IDE 1.14.1

Hi all,    basic info:    stm32 CUBE IDE v1.14.1    PC: Win10 64bit    MCU:STM32G0B1CC     In my code, there are two functions to control the battery to enter charge mode from init mode, when the battery receive a command. Check_AuthCmdToCHG()will se...

kevinKang by Associate II
  • 1918 Views
  • 3 replies
  • 0 kudos

Resolved! Slow down SAI Audio output

 Hello,I am currently programming an STM32F469I in STM32CubeIDE (I am a beginner with STM) and I am facing some issues.What I want: I want to read WAV file data from an SD card and send it to the AUX output so I can hear it on my headset/speaker. Cur...

LCKR register useage

Hi ,I am using the stm32f411VET MC board, now i implemented the code to check how LCKR register work. This is the code which i implemented for that, but when i debugged it the LCKR register bits has not set. Any one can help me. /** interfacing LED w...

suhel by Associate
  • 566 Views
  • 0 replies
  • 0 kudos

Resolved! LIve Exressions says " Failed to evaluate expressions.".

Hi.I am developing on STM32CubeIDE with F446RE Nucleo, and I want to get the voltage value by calculating ADC value.But that doesn't work.Here is the "main.c".I made two variables.(" ADC " means ADC value, " v " means voltage value.)Red texts are tex...

MED2972 by Associate III
  • 8986 Views
  • 14 replies
  • 8 kudos

debug SFRs

I can't read/change the SFR values while debugging in CubeIDE .value of all Registers is "error reading value"If I try to do that IDE throughs and error.The only way to read/change values is by suspending the debugging session.I remember this feature...

Screenshot 2024-11-14 133954.png 0693W00000NqiAGQAZ.png