STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1544 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! How can I add the [-Wenum-conversion] warning check?

Hello,How can I add the [-Wenum-conversion] warning check?If I check the "Warn for implicit conversion (-Wconsersion) I have many warnings from ST originated files (stm32l4xx.h) so I can not use this option....Best regardsMich 

mich35 by Associate III
  • 2059 Views
  • 4 replies
  • 0 kudos

Resolved! X-CUBE-MEMS1 Error: Board Part Number not defined

I have a Nucleo-H755Zi-Q and a IKS02A1. I am using the X-CUBE-MEMS1 Package. In the configurator, when I select "Board Extension IKS02A1"  I get the following error:#error "Board Pin number not defined!! Add USE_NUCLEO_144 define within stm32h7xx_nuc...

Resolved! The float formatting support is not enabled

Hello All,I am getting this error while compiling the project " The float formatting support is not enabled ".I have checked use float with "printf from new lib-nano" in MCU/MPU settings save and recompile the problem didn't go!!I have added manually...

Fahd by Associate II
  • 4921 Views
  • 4 replies
  • 4 kudos

Resolved! HAL_Delay() --> SysTick_Handler never be called

Hi all,Version: 1.15.1MCU : g473Before investigate deeply on my own I wonder whether if anyone have faced the same problem with Interrupt table in general ...I placed a breakpoint there :void SysTick_Handler(void){/* USER CODE BEGIN SysTick_IRQn 0 */...

bibah by Associate II
  • 3813 Views
  • 6 replies
  • 2 kudos

Resolved! serial monitor not working

im trying to create a project that write something in the serial monitor(raed/write) . i followed many tutorials step by step but i everytime my serial monitor doesnt print my message( i used tera term/putty/and even the serial monitor in the ide "co...

Screenshot 2024-07-09 115726.png
yessine by Associate III
  • 8905 Views
  • 9 replies
  • 2 kudos