STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1544 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How Wise Studio work????

Hi all, I'trying to explore steval board with BlueNRG2 chip, I'm working on BLE_SensorDemo project, works nice, right now I wan to develop my owm file, so far I've developped a library for SPI flash.I've added my header in Inc folder et my source fil...

SBaro.11 by Associate III
  • 1265 Views
  • 1 replies
  • 0 kudos

"Search" not working

Dear CubeIDE team,I just started using CubeIDE.Following are my question.1. How can I find string text in .h file?    I tried to "ADC_OVR_DATA_OVERWRITTEN" string in Drivers\..\inc using "Ctrl+H" but I failed.    This is very uncomfortable to use. No...

Tiel by Associate II
  • 2110 Views
  • 2 replies
  • 0 kudos

Resolved! H747i-DISCO programming/ creating binary

How would I be able to create a binary for this project or run it through CubeIDE? For some context I have taken this project from the FP-AI-VISION1_V3.1.0 pack, made some modifications, and would like to flash my H747i board with it. I can build the...

tw1_0-1732245633377.png
tw1 by Associate II
  • 1182 Views
  • 2 replies
  • 1 kudos

Suppress compiler warnings for library files

I'd like to configure GCC to suppress warnings from library files - e.g. I don't want to see the -Wconversion warning in stm32f4xx.h, but I do want to see all warnings from source files that I write myself.  I'm using STM32CubeIDE v1.10.1 on Windows....

STM32H533CET6 File download error

Hi everyone, I have problems programming the STM32H533CET6, I get a file download error.  Error: failed to download Segment[0] Error: failed to download the File Encountered Error when opening C:\ST\STM32CubeIDE_1.16.1\STM32CubeIDE\plugins\com.st.stm...

Resolved! Out of memory error.lwip

Good evening everyone; I was going to ask about something the size of it. If anyone has any information, I'd be happy. STMCube ide is also the LWip library tool. For MQTT connection via Ethernet. After publishing and subscribing for a certain period ...