Skip to main content
Senior
July 20, 2024
Solved

How to input non-numbers in timer configurations?

  • July 20, 2024
  • 1 reply
  • 715 views

Hi,

In various ST's example .ioc files, the timer PSC, period, etc, are set with text but not numbers. This will define the numbers to macros in the code. But I can't input text in the CubeIDE. So, is this feature only supported in the standalone version of CubeMX?

Thanks.

    This topic has been closed for replies.
    Best answer by diverger

    Got it. Just click the gear icon to the right, and select 'no check', then I can input whatever I want.

    1 reply

    divergerAuthorBest answer
    Senior
    July 20, 2024

    Got it. Just click the gear icon to the right, and select 'no check', then I can input whatever I want.