STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 564 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32 C++ CMake Project - Dual-Core Board

Hi all.While I found it really nice that CubeIDE offers the option to generate a CMake Project, it can only generate projects for one core. I have the STM32H757I Evaluation Board, which is M7+M4 and I can't create a project for both cores. The STM32 ...

nnoK by Associate
  • 734 Views
  • 0 replies
  • 0 kudos

Resolved! Erase the MCU

I am working on EEPROM emulation. I am programming flash frequently and may have mistakes in my code. When I take a break I'd like to erase the MCU so that I don't have bad code in there possibly wearing out the FLASH. Is there a way in the IDE to ju...

Carl_G by Senior III
  • 1523 Views
  • 2 replies
  • 1 kudos

Resolved! No ETH Connectivity Option for STM32F779

I cannot find the ETH connectivity option in the Pinout & Configuration window. It is listed as an option in the datasheet, and pins are given for the various MII options. What can I do to configure the MCU with a RMII interface to an external PHY ch...

jcGTRI_0-1740070191837.png jcGTRI_1-1740070353410.png
jcGTRI by Associate
  • 1284 Views
  • 3 replies
  • 1 kudos

Resolved! if-block brace ignored...why?

Hi guysIn the picture, you can see a code fragment in debugging mode. You also may see, that the controller is forced to stop at line 476, the if statement.Now the problem: I want to enter the if-branch, if the function returns with the READY typedef...

White_Fox by Associate III
  • 2754 Views
  • 4 replies
  • 1 kudos

STM32CubeIDE .cproject vs CMake files

Hello,I've started working with CMake in STM32CubeIDE: STM32CubeIDE Version: 1.17.0 Build: 23558_20241125_2245 (UTC) (C) 2024 STMicroelectronics ALL RIGHTS RESERVED Everything works perfectly, and I can compile without any issues.However, I'm not s...

Source Format function bug?

HelloI setup the IDE with the code format that I wanted under project preferences. Then I right click on the source code (*.c .h or dir), then get the context menu and select "Source"->"format.  This seems to reformat the code  as expected, but shoul...

matt-crc by Senior III
  • 1579 Views
  • 4 replies
  • 0 kudos

Changing CubeIDE Comment Color

Hi,I'm using STM32CubeIDE with the Dark theme and Default colors and fonts, and I can barely read the comments with the gray on gray color scheme (pictured below).  How can I change the color of the commented/inactive code sections?  I've gone throug...

Screenshot 2024-06-19 120600.png
hypoxic by Associate II
  • 5070 Views
  • 3 replies
  • 6 kudos