STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1436 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! i can't log in myST

This is the first time I use STM32cubeIDE ver 1.15.1 . While using it, there are a few operations that need to be logged in. I already have an account in the practice room at school, but when I log in on my personal laptop, I see a box. "Authenticati...

Screenshot 2024-05-14 171838.png
dnht by Associate
  • 10894 Views
  • 14 replies
  • 12 kudos

Resolved! elf has a LOAD segment with RWX permissions w/ Optimization

I upgraded my MacBook computer and installed the latest STM32CubeIDE 1.17 like many other people reporting the new warning that has appeared with the 12.3 toolchain.  I have an STM32F413 project I have been working on for a few years which uses an RT...

tlsvd by Associate II
  • 2894 Views
  • 5 replies
  • 3 kudos

STM32Cube IDE problem flashing the code

Hi, I'm able to build the project and generate the hex file. Out of sudden i'm not able to flash my board using STLink v2 neither i'm able to enter into debugging mode. Using STM32CubeProgrammer i'm able to flash the board but i want to enter into de...

ape07_0-1739940858190.png
ape07 by Associate
  • 1188 Views
  • 2 replies
  • 0 kudos

Log Values from STM32H747IGTX M7 Core on PuTTY

Hello, So right now I am trying to get my printf to work on CubeIDE and printing the respective output on PuTTY. I can't seem to figure out why it doesnt work when people on Youtube simply press run and their code works.For context... 1. Using M7 cor...

Goldylux by Associate II
  • 1618 Views
  • 4 replies
  • 1 kudos

We cannot connect. mail adress and dont see main c

"Hello, I am opening a new project in STM32 Cube IDE. When I create the project, the main .c files are not being generated. During the process, it gives the error shown below. When I try to log in with my email address and password to download the re...

STM32CubeIDE(Ver1.17.0) build link error.

When I build with STM32CubeIDE (Ver1.17.0), a link error occurs.I am attaching an excerpt from the log file about the error that occurs at this time. (Only after the "Failed" part of the log)Strangely, even if the above error occurs, the .elf file is...

k_kato by Associate II
  • 1034 Views
  • 0 replies
  • 0 kudos

Use 7zip and SRecord in CubeIDE project

Hi all,I would like to know how to add the packets 7zip and Srecord in a CubeIDE project.I'm working on a project I didn't start and after compiling the IDE returns the error messages "7z is not recognized as an internal command" and "srec_cat is not...

ALuiz.1 by Associate II
  • 1994 Views
  • 3 replies
  • 0 kudos