STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1121 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 481 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE(Ver1.17.0) build link error.

When I build with STM32CubeIDE (Ver1.17.0), a link error occurs.I am attaching an excerpt from the log file about the error that occurs at this time. (Only after the "Failed" part of the log)Strangely, even if the above error occurs, the .elf file is...

k_kato by Associate II
  • 1021 Views
  • 0 replies
  • 0 kudos

Use 7zip and SRecord in CubeIDE project

Hi all,I would like to know how to add the packets 7zip and Srecord in a CubeIDE project.I'm working on a project I didn't start and after compiling the IDE returns the error messages "7z is not recognized as an internal command" and "srec_cat is not...

ALuiz.1 by Associate II
  • 1916 Views
  • 3 replies
  • 0 kudos

Resolved! STM32CubeIDE Compile Time using Linux is VERY SLOW

Since upgrading to 1.17.0 compile times have went from a pleasant time to wow, that is slow.  Anyone else experiencing this?Basic project from template: 22:45:47 **** Incremental Build of configuration Debug for project CompileTimeTest **** make -j4 ...

Missing or incorrect documentation for CubeIDE v1.17.0

Where can I find the correct manual for the CubeMX module contained within the CubeIDE v1.17.0. Specifically looking for info on the Project Manager/Boot Project Checkbox and how to disable the creation of the Boot Project seen in the Project Explore...

dbrooks by Associate II
  • 649 Views
  • 0 replies
  • 0 kudos

UChar.h is missing

Hi,I just found out <uchar.h> is missing from standard c header files in \STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.1.0.202410251130\tools\arm-none-eabi\include. How am I supposed therefore to u...

GMeur by Senior II
  • 2278 Views
  • 4 replies
  • 1 kudos

Resolved! Problem opening a project CubeIDE

Win 10, x64, STM32CubeIDE version 1.17.0I'm trying to open a CubeIDE project from a workspace but it just doesn't load, see image below. I select the folder for my workspace, click finish & am then told that there are no projects in the folder. Yet t...

Cube_Proj_Issue.png

Resolved! stuck on creating a new project from ioc file

I'm trying to create a new project from a exiting ioc file.When I click the "finish" button, it shows a progress bar but disappear very fast, and it did nothing else. No new project created, no nothing. I don't know what went wrong. Is there an error...

soapshepard_0-1739770170418.png

Tips for debugging programs with CubeIDE

Please listen to the trouble and cause when debugging with CubeIDE that I was troubled withThe cause is very simple once you understand it, but I couldn't think of it at the time of trouble. Details of the trouble A CubeIDE sample program was execute...

Kiyama by Associate II
  • 1257 Views
  • 0 replies
  • 1 kudos