User Activity

Hello.We need to use g++ linker in our project.But after setting g++ linker in Project->Properties->C/C++Build->Settings->MCU G++ Linker to g++ again ld.exe is invoked.Would you please advice.Thank you.
Hello.We are using PA3 pin as input with pin pull up enabled.Power consumption of the board is around 36 microamps when pin is not connected to ground.But when we connect PA3 to ground we have current increase to 74 microamps.I think that we have som...
Hello.How can we enable brown out for this processor and the brown out voltage?Thank you.
Hello.We are trying to read measured voltage by MAX17201 chip - register 0x09.But we are receiving incorrect value - 0x936A when battery voltage is 3.0V?!We are using I2C communication protocol.Here is the I2C initialization:static void MX_I2C1_Init(...
Hello!We are trying to add some header files to a project loaded in STM32CubeIDe.We are setting new files path via this menu - “Project ! Properties ! C/C++ General ! Paths and Symbols ! Library Paths�?Files are in specified directories but when we t...
Kudos given to