User Activity

Hi,I tried installing ARM Cmsis 6 Pack with STM32CubeIDE 1.16.1. It is having errors. I'm attaching the screenshot below -Though ARM Cmsis 5 is working fine.!
(originally a reply to https://community.st.com/t5/stm32cubeide-mcus/retarget-printf-on-stm32g070rbxx-cortex-m0/td-p/720883) Hi @Andrew Neil,For the scanf do we need to make any other change?My read function is-  int _read(int fd, char *ptr, int len)...
Hi,I'm trying retarget printf. My uart_write function is working correctly and i'm able to see character on Teraterm.But when i try to use printf it is not working. i even tried semihosting to execute printf but it fails. i'm attaching the screenshot...
Hi,I have created a project using STM32CubeMX and Keil uVision.The generated CubeMX comes with its own main.c and main function.What I want to do is disable that main.c build in the project and create my main.cpp file,where I can put my main function...
When i try to connect g070rb nucleo board i get my LD1 blinking continuously and on my pc it shows usb device not detected​.
Kudos from
Kudos given to