STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Build terminate with exit code -1.

Hi All,I compiled my code, no error no warning, but I get this code below. Also, when I try to run the code, it is not uploaded to the board.Could you pls check for me ? **** Incremental Build of configuration Debug for project Boot ****make -j8 all ...

demir by Senior II
  • 4215 Views
  • 4 replies
  • 0 kudos

SWV Trace not working in C++ projects

I am having problems using SWV options with c++ projects, using a Nucleo F767ZI board.I tried using SWV data trace with a simple C project and everything works fine, however (using the same configuration I used in the C project) I couldn't get any ou...

FDi L.228 by Associate II
  • 1261 Views
  • 1 replies
  • 2 kudos

Resolved! Ubuntu 24.04 install of Cube IDE 1.15.1

When moving to the latest LTS version of Ubuntu (version 24.04), I received the following message when attempting to install Cube IDE and after accepting all of the license agreements:The following packages have unmet dependencies:st-stm32cubeide-1.1...

w3dmj by Associate
  • 34171 Views
  • 20 replies
  • 13 kudos

Resolved! Linked Files

I'm working on a project that will be using shared code files from outside the project.  I do not want to copy them, instead I want to link to them.  I discovered how to do this and it works well.  Since I don't want to make any changes to any of the...

RLein.1 by Associate III
  • 3966 Views
  • 12 replies
  • 5 kudos

Connect to running GDB server without ST-Link

I am trying to debug a program in STM32CubeIDE on a Renode emulator, with a running gdbserver, started by Renode.So in Debug Configurations dialog, Debugger tab, there is a radiobutton Connect to remote GDB server, but when clicking Debug, it complai...

SKled.1 by Senior II
  • 7067 Views
  • 10 replies
  • 2 kudos