STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Flash SR errors on startup

Hi all.I'm working on stm32WB MCU, I have a bootloader and an application. The bootloader only check if any update needed and jump to app. When app stops at main I can see that flash status register is set with PGAERR, SIZERR and PGSERR and I have no...

YWor.1 by Associate III
  • 904 Views
  • 0 replies
  • 0 kudos

STM32 WB09KE - Emulate EEPROM from flash

Hello everyone, I am currently working with the STM32WB09KE microcontroller and need to implement EEPROM emulation, as this device does not have built-in EEPROM. However, I couldn't find specific documentation or resources related to EEPROM emulation...

rlopes by Associate III
  • 1050 Views
  • 2 replies
  • 0 kudos

Resolved! Lora Relay Node

Hi,Anybody from ST or Users done any development or research on the "new" relay node on the STM32WL.Will the stack be updated or will we have to do this on our own?RegardsStefan

tech2399 by Associate II
  • 3033 Views
  • 5 replies
  • 2 kudos

Resolved! After BLE OTA update, CPU2 stucks

Hi, I'm working on an OTA BLE bootloader for the STM32WB5MM module.I created from scratch with STM32CubeMX the same code as the OTA example for NUCLEO-WB55.I'm on BLE stack 1.21So far so good, I can update with the smartphone app.The problem I'm havi...

PCu1 by Senior
  • 3488 Views
  • 5 replies
  • 2 kudos

STM32WB15 FUS refusing to start

I was updating application firmware on an STM32WB15CC, but my user application wasn't advertising correctly.  I decided to re-install the wireless firmware.  However, I am unable to do so, as my FUS refuses to start.  Reading the FUS infos shows a FU...

ironduck_0-1741364212601.png ironduck_1-1741364260797.png
ironduck by Associate
  • 783 Views
  • 1 replies
  • 0 kudos

STM32WL54 does not wake up after 4-5 days in STOP2 mode

The device is designed i  a way that, it should wake up every 30 seconds via RTC wake up timer or upon button press, read sensor values (for temperature and humidity ), if there is any change in these values , send packets via radio (SUBGhz) and ente...

euclid by Associate
  • 1843 Views
  • 2 replies
  • 0 kudos

Resolved! Setting SC_KEY_TYPE to debug mode fails in STM32WB55

Hello, I want to enable the secure connection key type as 'DEBUG' in STM32WB55 with my custom setup. The cube IDE does not allow this setting in the configuration of .ioc file. I followed this tutorial and added the following line in my code inside t...

tmk_0-1739237869435.png tmk_1-1739238012604.png
tmk by Associate II
  • 1179 Views
  • 2 replies
  • 0 kudos