Skip to main content
OliM
Senior II
September 19, 2024
Question

Confusing STM32WB0 prices

Looking through the WB0x portfolio, it looks like the WB06 and WB07 VFQFPN are completely unattractive and even the WLCSP not a good bargain.
STM32WB06KC is supposed to be 1.87 Dollars, whereas STM32WB09KE stands at 1.013 Dollars.
Also the later would actually make a *** of the stm32U083KC as long as you don't need USB, since it is supposed to use less power, has double the Flash, more RAM (and BLE of course) and costs 25% less.

Actual listings at DigiKey and Mouser back up the budgetary claims. So what's up with those prices?
EDIT: Really, you censor the word F o o l ?

This topic has been closed for replies.

1 reply

Billy OWEN
ST Employee
September 19, 2024

Hi @OliM 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy