STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 234 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4076 Views
  • 0 replies
  • 3 kudos

Resolved! Setting SC_KEY_TYPE to debug mode fails in STM32WB55

Hello, I want to enable the secure connection key type as 'DEBUG' in STM32WB55 with my custom setup. The cube IDE does not allow this setting in the configuration of .ioc file. I followed this tutorial and added the following line in my code inside t...

tmk_0-1739237869435.png tmk_1-1739238012604.png
tmk by Associate II
  • 1204 Views
  • 2 replies
  • 0 kudos

Resolved! Accepting / rejecting pairing requests on STM32WB55

Hello, I am using STM32WB55 chip on my custom setup. I have configured my device in peripheral mode. I want to be able to accept / reject pairing requests initiated by the client device. I am following AN5270 for development. I have added code to set...

tmk_0-1741228230220.png
tmk by Associate II
  • 891 Views
  • 1 replies
  • 0 kudos

HCI_COMMAND_COMPLETE_EVENT ON STM32WB55

I am using the stm32wb5x_BLE_Stack_full_extended_fw.bin (1.18) on my STM32WB55. I would expect to get the HCI_COMMAND_COMPLETE_EVENT after calling hci_reset(), but I never get the event. I get the other HCI events such as HCI_DISCONNECTION_COMPLETE_E...

Resolved! TX power Level in BLE Advertisement

Hi allWe are using STM32WB55 for BLE application. By default, the TX power is added to AD data structure. Got to know that we can use this below API to remove the field from advertisement. ret = aci_gap_delete_ad_type(AD_TYPE_TX_POWER_LEVEL);Is there...

ABN_0-1740402584432.png
ABN by Associate III
  • 1521 Views
  • 2 replies
  • 0 kudos

FUS and Wireless Stack Programming Error

HelloI'm working with a custom STM32WB55RG board which initially was working properly, reading documentation regarding failures and STM32WB Firmware Upgrade Service upgrade.I tried to upgrade and follow the steps indicated, I also tried to follow sev...

Daniel_RH_0-1737581985974.png Daniel_RH_1-1737582063880.png Daniel_RH_5-1737582190901.png Daniel_RH_4-1737582173734.png
Daniel_RH by Associate II
  • 3318 Views
  • 9 replies
  • 3 kudos

STM32WLE5 core current consumption and NVM protection

Hello Everyone,I am working on STM32WLE5CC and I am new to this. I am getting current consumption of 520uA of Core only in which I have initialized HAL_Init() and   SystemClock_Config() with MSI of 1MHz. And datasheet states that in Active mode it ta...

Ronik_123 by Associate II
  • 1511 Views
  • 2 replies
  • 0 kudos