MEMS (sensors)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MEMS-Studio FSM on MKI109D

Hi, I have the STEVAL-MKI109D board, on which I mounted the STEVAL-MKI250KA. I would like to implement the free-fall example on the FSM, using data from the ST1VAFE3BX biosensor, using only MEMS Studio. Is it possible to do this without writing firmw...

Resolved! How to integrate driver for iis2mdc magnetometer

Hi all,I need to integrate the driver for the iis2mdc magnetometer (Github: https://github.com/STMicroelectronics/stm32-iis2mdc/tree/main) into my own project for a custom board (with STM32H7A3 and i2c3).  The code from the driver requires an additio...

GS1 by Senior III
  • 42 Views
  • 1 replies
  • 0 kudos

How to set up and read SFLP Game Vector on ISM330BX

Hello,I am developing a custom application that uses your ISM330BX IMU. I am communicating with the IMU using I2C. I checked that I can commuicate correctly with it by requesting the ID in the WHO_AM_I register and everytihng seems to work fine.The e...

Integrating MotionFX: Gives random data

We've implemented an example program based on UM2220 using an lsm6dsox IMU sensor on an STM32U575 microcontroller. We're trying to use MotionFX for orientation calculation from 6 axis measurement, configured with accelerometer and gyro. The IMU senso...

ISM330DHCXTR power on time

Hi I'm working with the ISM330DHCXTR sensor and would like to know how long I should wait after applying power before the device is fully operational and ready to communicate (e.g., via I²C) Thanks Uri

Uri_m by Associate
  • 27 Views
  • 0 replies
  • 0 kudos

Resolved! SensorTile.Box PRO and STEVAL-MKI168V1

Hi, I have an evaluation board STEVAL-MKI168V1 with the sensor IIS2DH. I was hoping to plug it into the DIL24 connector of the SensorTile.Box PRO and be able to see the sensor's output using the MEMS Studio. This does not seem to be the case. Can som...

msv by Associate
  • 55 Views
  • 1 replies
  • 0 kudos

Convert I3G4250D gyro raw output to understandable values

Hello STM32 community,I'm relatively new to STM32 development and I'm currently working with the I3G4250D Gyro Sensor on the STM32F411e-Discovery board. I've been using the stm32f411e_discovery_gyroscope.c file (BSP Drivers) provided by STM32Cube to ...