MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Support to build a device with multiple IMUs

Hello All,Apologies in advance for sounding like a noob (that is because I am). I am building a wearable device as a hobby, and I need a 6-axis gyroscope with IMU. Ideally, the device should have more than one IMU, but considering that I have absolut...

ISS2MDC High Power Consumption on Idle

Hello,I am evaluating the STMicroelectronics IIS2MDC magnetometer and measuring its supply current using a Joulescope. According to the datasheet, the device should draw approximately ~1.5 µA in idle mode, yet I consistently measure about 450 µA, whi...

Starter Package for NTM88 and MKW01

Hi, I am working on a TPMS project and I have migrated from FXTH to NTM88. With the FXTH I was using the MKW01 board for RF communication, on the NTM88 side, to use the same RF board I need the Starter Package for NTM88 and MKW01. The link can be fou...

mnicolae by Associate
  • 234 Views
  • 3 replies
  • 5 kudos

LIS2MDL magnetometer with steval_mki181v1

Hello everyone,I'm working with the LIS2MDL sensor (steval_mki181v1) , i made a connection between it and the nrf5340 and I configured it over I2C with pull-up resistors enabled.-VDD -- > VDD-VDDio --> VDD-CS --> VDD -PIN I2C  :: SCL to SCL et SDA to...

ASREB_0-1777298804785.png ASREB_1-1777298856405.png
ASREB by Associate II
  • 734 Views
  • 17 replies
  • 1 kudos

IIS2MDC INT/DRDY configuration when unused

Hello,  I am currently using the IIS2MDC in my design with the following configuration: As you can see, I am not using the INT/DRDY pin, so it is left unconnected. However, in idle mode, I am measuring an abnormal current consumption of around 400 µA...

npreel_0-1779094713447.png
npreel by Associate II
  • 133 Views
  • 0 replies
  • 0 kudos

LSM6DSV16X pitch/roll signal anomaly

Hi,We are using a LSM6DSV16X unit to track pitch and roll in our product based on the quaternions reported by the unit's SFLP algorithm (High Accuracy ODR 120Hz)During the operation and in what seem to be arbitrary times, the pitch and roll signals f...

145018_RightLeg_IMU_error_roll_detail.PNG
JoanV by Associate II
  • 728 Views
  • 14 replies
  • 0 kudos

Resolved! LSM6DSO I3C SETDASA

Hello!I'm working on an Nucleo-H503RB board and trying to communicate with a LSM6DSO over I3C.I am now able to use ENTDAA to assign a dynamic address to the LSM6DSO.Next, I want to test using SETDASA to assign a dynamic address based on the static ad...

jad1_0-1777514154625.png jad1_1-1777514179063.png jad1_2-1777514187310.png
jad1 by Associate II
  • 506 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.