MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using X-CUBE-MEMSMIC1 without X-NUCLEO-CCA02M1

Hello, I am trying to record audio with external digital PDM microphones using the MEMSMIC1 example but it is not so straightforward without the nucleo expansion board. Because the CCA02M1 has a direct connection to the pc it is able to be detected a...

[MEMS Studio] HPF feature bug

Hi,I've tried to use high-pass filter in MLC in MEMS Studio, but the results are incorrect for first windows in each data file. I found that result is different from the one from Unico, but probably because Unico just drops first 2 windows from each ...

tomny_0-1769093543815.png
tomny by Associate II
  • 104 Views
  • 1 replies
  • 1 kudos

Resolved! ISM330DHCX INT1 to LDO EN pins

I need to save power in a project; the system will turn on when shaken. I need to configure INT1 pin to leave the LDO open for 15-20 seconds. Conditions:1- Did the device move? (acceleration)2- Are the x, y, and z axes in the correct position?If cond...

YBAYR.1 by Associate III
  • 135 Views
  • 3 replies
  • 2 kudos

Resolved! LIS3DH footprint discrepancy

Hello ST Community,Based on a photo found on the internet of the LIS3DH chip and a comparison with the package information in the datasheet, I found a discrepancy in the footprint.The datasheet appears to show the pin-1 mark on the opposite side comp...

GALS_0-1769007094007.png GALS_1-1769007460878.png GALS_2-1769008479126.png GALS_3-1769008503511.png
GALS by Associate II
  • 95 Views
  • 2 replies
  • 2 kudos

9-axis sensor fusion implementation DT0058& DT0060

Hi Sir,1. Regarding Initialization (Absolute Orientation)In my application, I need to obtain an absolute orientation (Roll, Pitch, and Yaw) relative to the Earth's frame. Is my understanding correct that the Initial Quaternion must be computed using ...

TIENHUA by Associate III
  • 101 Views
  • 1 replies
  • 0 kudos

Resolved! lsm6dv320x odr-triggered mode not working

Hello, I'm trying to use ODR-triggered to get data aligned with my clock. I'm sending a square wave 50% duty cycle period 2000ms over INT2 pin, yet when I poll the IMU every 50 ms the accel and gyro data changes, even though it should be aligned to t...

rulmer_0-1769011277205.png
rulmer by Associate
  • 87 Views
  • 1 replies
  • 0 kudos

LIS2DU12 wake up configuration

Hi everyone,I'm using 2 LIS2DU12 on one object.The first one is configured in continuous mode. I forward the samples directly to a computer. I use it to check the wake up triggering configuration of the second one.The second one is configured in cont...

Ch4rly by Associate II
  • 528 Views
  • 5 replies
  • 0 kudos