MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

finding location without GPS

I am currently working on a project involving the SensorTile.Box and am seeking assistance with utilizing its gyroscope and accelerometer sensors to determine location in the absence of GPS signals. Specifically, I am interested in processing the sen...

Eneasy by Associate
  • 2437 Views
  • 2 replies
  • 1 kudos

Resolved! ISM330DHCX I2C issue

Hi,I'm evaluating the ISM330DHCX by connecting it on a board with a linux device (imx8) through I2C. (using the st_lsm6dsx - (compatible = "st,ism330dhcx") device.All of this seems to work out of the box, and I can read accelerations through IIO sysf...

ArnoutDekimo_0-1721829511164.png ArnoutDekimo_2-1721829799447.png ArnoutDekimo_3-1721829824422.png ArnoutDekimo_5-1721834361984.png

Resolved! Strange whoamI value LSM6DSO32

Hi allI'm working with an STM32F405 and one LSM6DSO32 and one LIS2DU12, eveyrthing works fine, but sometimes, for unknow reason, I go a strange whoamI from my captor, I got 0x20 value, I reset my mcu and it's works fine, any idea ? For my driver I us...

SBaro.11 by Associate III
  • 3801 Views
  • 7 replies
  • 1 kudos

Resolved! Unico GUI Meta-classifier Issue

I am using LSM6DSOX for my project. As far as I understand, meta-classifiers need to be separate for each function (for my project). But I cannot separate two_hands_free and pushing_chart functions. I think this would pose a problem for machine learn...

Ekran görüntüsü 2024-07-29 162602.png
ttugur by Associate
  • 1413 Views
  • 1 replies
  • 1 kudos

Wake-Up current of IIS3DWB

I am making my own wake up interrupt program based on P16 of the application note, and it is working fine. However, I noticed that I have to enable IIS3DWB to use the wake up function, which increases the overall standby current of the system by abou...

chenjy96 by Associate
  • 781 Views
  • 0 replies
  • 0 kudos

Error in raw data IIS3DWB

Hello, I am encountering strange samples in the raw data using the IIS3DWB accelerometer. I can make several requests for raw data without issues, but at a certain point, I receive data with incorrect values at specific sample positions. Whenever an ...

GThabet by Associate II
  • 3226 Views
  • 3 replies
  • 0 kudos

LSM6DSL Accelerometer data deviation

Hi,We are using LSM6DSL for one of our products and in that we have noticed that the Z-axis Accelerometer deviates due to change in temperature for a stable orientation as shown below which is affecting pitch of the product  by -1 to -2 deg.    The I...

harishsingh_8-1722257653405.png harishsingh_9-1722257677455.png harishsingh_10-1722257699554.png harishsingh_0-1722259424722.png

Resolved! VL53L1X Calibration Offset

Hi,I am fighting with the offset calibration of multiple VL53L1X. I use the API ULD with Arduino.I build a device to have 4 sensor[4] at 140mm far from a same plan. 2 of them give a good measure, 2 of them do not.I have tried the following process to...

OTELL.1 by Associate
  • 2807 Views
  • 3 replies
  • 0 kudos

IKS4A1 sensor axis information ?

Hello, I'm desparately trying to find a diagram that would explain how the different sensors (accelerometers, magnetometer, gyros...) are oriented on the IKS4A1. We can find individual axis information for each sensor on their specific datasheet, but...

AnselmeC by Associate II
  • 1909 Views
  • 3 replies
  • 0 kudos