MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How config IIS3DWB to FIFO mode with Watermark?

Hi, I'm trying to use the IIS3DWB as FIFO mode with a watermark.I'm using a custom board. I double checked the hardware and guaranteed this board works well. I'm able to read/write the sensor using SPI interface and generate interrupt with wake-up in...

uilter by Senior
  • 2607 Views
  • 3 replies
  • 0 kudos

Resolved! Are LIS2DW12 registers non-volatile?

I want to setup the wakeup configuration registers and then disconnect the accelerometer from an I2C programmer and power source. When the accelerometer is placed with the new circuit, will the configurations in the register I have set still remain? ...

Lab1tr by Associate II
  • 1024 Views
  • 3 replies
  • 0 kudos

Unable to get distance measurements from VL53L3CX

I'm using an ESP32 to communicate with the VL53L3CX. I successfully reworked the vl53l3cx_platform.c file to get communication working with the sensor using I2C, which is a good start. But when I go to read from the sensor (using polling, not hardwar...

0693W000005C09vQAC.png 0693W000005C09LQAS.png
NSack.1 by Associate
  • 3518 Views
  • 4 replies
  • 0 kudos

IIS3DHHC sensor and (Extended) Kalman Filter (EKF)

Hi, I try to use IIS3DHHC as a simple inclinometer. I learnt that to get stable readings it may be a good idea to process raw data using Extended Kalman Filter (EKF). Some ST demonstrations available on YT mention that as well, but I found no source ...

TDJ by Lead
  • 2151 Views
  • 2 replies
  • 1 kudos

Resolved! Implementation for MEMS1 librairi : don't work !

Hi,i am using ism330dhcx and lis2mdl on my custom board,i am able to configure and read data from accelero, gyro and magneto.i started the implementation of X-Cube-MEMS1 lib.when i compile the code, every thing is ok,but after running, when a functio...

malarab_0-1724321994996.png malarab_1-1724322019406.png malarab_2-1724322046678.png malarab_3-1724322172683.png
malarab by Senior II
  • 1192 Views
  • 1 replies
  • 1 kudos

LIS2DH threshold calculation problem

Hi everyone, I want to ask about the LIS12DH threshold calculation (attached with what I think the calculation is), it is clear that when I use 4g as the scale, my calculation results are 2.5g, when I move the sensor can go above this threshold and t...

jokerlove_0-1724235066350.png image.png
jokerlove by Associate II
  • 1654 Views
  • 2 replies
  • 1 kudos

X-CUBE-MEMS1 application Inclinometer and eCompass

Hello,      on a custom board which mounts STM32F407 CPU with LSM6DSV16XTR accelerometer+gyroscope and LIS2MDLTR magnetometer I have to implement an inclinometer and a eCompass with the maximum accuracy. Now, it is not completely clear to me how to g...

MRaff.1 by Associate III
  • 1031 Views
  • 0 replies
  • 0 kudos

STM32L496ZG +MPL3115A2 interface

I am using STM32L496ZG nucleo board for interface MEMS MPL3115A2 Sensor using I2C interface . First i am scanning I2C device and find attached device too.But after scanning device whenever i tried to read Who am i register , i don't receive correct...

0693W000003QtjUQAS.png 0693W000003QtkXQAS.png 0693W000003QtkmQAC.png 0693W000003QtnlQAC.png
RPate.4 by Associate
  • 2831 Views
  • 4 replies
  • 0 kudos

Resolved! LSM6DSO Pedometer

Hi BenG142, I'm trying to develop a pedometer application using the LSM6DSOX sensor, but I haven't been successful. Could you share your project files with me? I'd like to know which registers you used. 

LPS27hhtw failure mode

Hi, I look on different application notes linked to the LPS27HHTW but I found nothing about its failure mode.I want to know what could be its failure mode and how will it react for eg on SPI communication (value at 0 or minimum or sea level pressure?...

David45 by Associate II
  • 1540 Views
  • 2 replies
  • 0 kudos