MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Microphone self noise IMP34DT05

Hello,I'm using the IMP34DT05 microphone and it records fine but there is always a noise overlapped and it is very annoying.I have tried recording the background noise in anechoic chamber (see attached audio, high-pass filter alpha is 0.98). Do you k...

frnt by Senior
  • 1314 Views
  • 2 replies
  • 0 kudos

Resolved! STW56N60DM2: Isolated back tab, or connected to drain?

Hello all,   I'm looking at the datasheet for the STW56N60DM2, and it's really not clear if the back of the FET is electrically isolated from the Gate, Source, and Drain. Typically, this is more clear in other datasheets I've looked at. Below is the ...

JW2112_0-1715867542156.png JW2112_1-1715867707583.png
JW2112 by Associate II
  • 4960 Views
  • 11 replies
  • 1 kudos

Sensor tile box

We got Sensor tile box and they were working fine until we uploaded this:https://www.st.com/en/embedded-software/stsw-mksbox1-bl.html/1000vai bluetooth. Now they are not visible on the app ST ble sensor. How to update the original firmware on the sen...

plawat by Associate III
  • 601 Views
  • 0 replies
  • 0 kudos

Resolved! How do you install PDM library ?

I struggle to use PDM Filter library.This is the message error I get : What I have done so far are : - in project properties, C/C++ general, Paths and syombols, in "Includes" I added the path to pdm2pcm_glo.h ; in "Library Paths" I added the path to ...

0693W00000KbhBQQAZ.png 0693W00000KbhEyQAJ.png
EEnco.1 by Associate III
  • 4884 Views
  • 10 replies
  • 1 kudos

LSM9DS1 with linux kernel 6.1.46

Hello,We have been using the LSM9DS1 in our own design with Linux kernel 4.19.x by adding drivers from ST github, and using the iio_generic_buffer tool to read values.Now we are upgrading to linux kernel 6.1.46 and I have checked that the drivers are...

Angel1 by Associate II
  • 1096 Views
  • 2 replies
  • 0 kudos

CS control LIS2DH

In the project I use Attiny13a) + LIS2DH SPI interface. One leg of the microcontroller is missing. Is it possible in SPI mode to connect the CS pin directly to GND, and not to the microcontroller port.In I2C mode there are enough pins, everything wor...

Artem777 by Associate
  • 658 Views
  • 1 replies
  • 0 kudos

LSM6DSO32 resonance frequency

Hello there,What is the resonance frequency of the LSM6DSO32 accelerometer and gyroscope?It is not available in the datasheet. I tried to open a customer support tickets but they just forwarded me to this forum. 

mk390d by Associate
  • 681 Views
  • 1 replies
  • 0 kudos