MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SensorTile.Box PRO asks Bluetooth Code

When I connnect sensorTile.box from App.the followign msg poped ip continuously. and no fucntion work properlywhat is the reason. I upgraded the FW on FOTA  at the first connection.what is the suggestion ?Thanks!Forest  

forestxu_0-1718761080315.png
forest xu by Associate II
  • 1049 Views
  • 5 replies
  • 0 kudos

ML implementation in ISPU

Can anyone provide a documentation over integration custom ml algorithm in ISPU.If I have a machine learning model like tflite or onnx how can I deploy it in ISPU

Amith_lal by Associate III
  • 1315 Views
  • 3 replies
  • 2 kudos

ISM330DLC Low Power Mode

Trying to get the lowest power out of this device, but it seems to draw at least 900uA of current when even the accel and gyro are disabled. Any suggestions on how to get the current draw of this device lower? Here's my setup:Custom PCBnormal current...

NSmit.9 by Associate II
  • 1121 Views
  • 3 replies
  • 0 kudos

Unicleo gui not detecting IKSO1A2

Hello, I'm learning how to use stm32 hardware and how to program it and today i connect the X-NUCLEO-IKO1A2 to my board (Nucleo-GO71RB) and installed the inucleo software,  i did everythink like te st video said, but for some reason the software does...

Fxpires by Associate
  • 741 Views
  • 2 replies
  • 0 kudos

Android HAL for LSM6DSOX sensor

Hello experts,I am using rock chip board with android 12 on it along with the sensor lsm6dsox connected on i2c2.I have added the driver and compile the Linux and then build android images.After booting I can see device is detected on i2c and probed s...

amol4394 by Associate
  • 889 Views
  • 1 replies
  • 0 kudos

Resolved! STHS34PF80: No data

Hi,we have designed a custom board that includes a STHS34PF80 but after triggering a one-shot acquisition, the DRDY bit is never set and reading from the TOBJECT_x and TAMBIENT_x registers without waiting for DRDY only returns 0. We are interfacing t...

NorSen_42 by Associate II
  • 1559 Views
  • 5 replies
  • 0 kudos