MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IIS2DLPCTR ODR Accuracy

Could you please provide information about the output data rate (ODR) for the IIS2DLPCTR accelerometer?For example, if I want an ODR of 50Hz in High Performance mode, with BW=ODR/2, how accurate is the 50Hz ODR?  Similarly, if I use the single data c...

NBerr.1 by Associate II
  • 937 Views
  • 3 replies
  • 0 kudos

calibration of accelerometer and gyro in lsm6d

we are using LSM6DSV16x sensor with nrf5340 dk board , wea are getting values like this ACC[mg]:x:-157.50,y:-30.74,z:981.00GYRO[mdps]:x:-700.00,y:-140.00,z:420.00,please help in calbration to get accurate values of  sensor .

AlgoBuilder for IKS01A2

Hi, I understand IKS01A2 is not supported anymore in the current AlgoBuilder software versionIs it still possible to download the last AlgoBuilder version that supports this board ?I can only download the latest version from the website (no older ver...

mtzt by Associate
  • 608 Views
  • 1 replies
  • 0 kudos

Resolved! What's best and way to calculate velocity from acceleration for IIS3DWB and what degree of accuracy should one expect with IIS3DWB accelerometer?

I am using IIS3DWB for machine condition monitoring product development project.I am using the below integration for velocity conversion as per MotionSP but unable to estimate speed RMS (not even 50% closer to the reference values).------------------...

AGosw.3 by Associate
  • 3386 Views
  • 7 replies
  • 1 kudos

Resolved! issue with NRF24L01 on STM32F07VET6 blackboard

I've been trying to interface the STM32F407VET6 with the NRF24L01 modules, however after trying multiple boards modules and library's it still fails to work. im not sure the issue is with hardware as ive tried multiple modules and the black board has...

voxe by Associate II
  • 1272 Views
  • 1 replies
  • 0 kudos

IKS02A1 and Nucleo H503RB don't work

Hi, I am curretly using a Nucleo H503RB and the IKS02A1 expansion board in order to use the ISM330DHCX.I tried several way to use via STM32Cube IDE which is my goal as i want to use C language without success to see any sign of an i2c adress with an ...

matkergo by Associate
  • 1301 Views
  • 1 replies
  • 0 kudos

How can I make BLE work on STWINKT1?

Hi,I am trying to use the BLE (SPBTLE-1S chip) on my STEVAL-STWINKT1 board. The idea was to use a project example from X-Cube-BLE2 with the following configuration :HCI_TL : BasicHCI_TL_Interface : UserBoardApplication : SampleAppI used the SPI2 to c...

KaisBo7 by Associate II
  • 1026 Views
  • 3 replies
  • 0 kudos

IIS2DLPCTR Internal LDO

I am thinking of powering the IIS2DLPCTR accelerometer VDD rail from a buck converter and wanted to understand if this part uses an internal LDO to step the VDD voltage down to power the internal MEMS block and ADC? Or does it use the supplied VDD di...

NBerr.1 by Associate II
  • 680 Views
  • 1 replies
  • 0 kudos