MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

About the use of STEVAL- MKBOXPRO in Japan

  I BOUGHT STEVAL- MKBOX PRO AND AM THINKING OF USING IT. I have a wireless function, but please tell me the status of technical conformity approval for use in Japan. There was no conformity mark on the package.

Hidee_O by Associate
  • 749 Views
  • 0 replies
  • 0 kudos

Predictive maintenance - STEVAL-STWINCSV1

I am using the FP-IND-PREDMNT1 STM32Cube function pack for predictive maintenance in STEVAL-STWINCSV1 board, which performs vibration analysis using a 3-axis accelerometer (3 DoF). My use case involves motor vibration analysis. Would it be beneficial...

buelaraj by Associate
  • 1404 Views
  • 1 replies
  • 0 kudos

Resolved! Quick start Rotating dice

HiI have a custom pcb design with a lsm6dsv and lsm303agr. So far it is only streaming xyz coordinates.I need to come up with something like a rotating dice in this Video at minute 5:20 :https://www.youtube.com/watch?v=1mV_L-KEMy0In fact i need to Sh...

MK..1 by Senior
  • 1178 Views
  • 1 replies
  • 0 kudos

Resolved! LSM6DSO - Interrupt Trigger

Hi,     Is there a way to perform a wake-up interrupt using the LSM6DSO, based around gyroscopic data instead of accelerometer data?  thanks 

Dude by Associate III
  • 1110 Views
  • 1 replies
  • 0 kudos

LIS2DW12TR IC capacitance

1) What capacitance does the LIS2DW12TR introduce to the I2C bus lines?2) What is it's maximum bus capacitance threshold in normal I2C mode (100khz)?The datasheet doesn't have info on either of these points. It only quotes that the max bus capacitanc...

Sensitivity of LIS2DW12 Accelerometer

GreetingsI am working with the LIS2DW12 accelerometer. I am using the device in Low Power Mode 1, with a FS = +-4g.According the application note AN5038, page 15, it says that the Low power mode 1, entails a 12 bit value. Thus, using the 16-bit value...

ZAIDS-S23 by Associate III
  • 1178 Views
  • 1 replies
  • 0 kudos

Is LSM6DSL Zephyr driver compatible with LSM6DSM?

Hello,Our custom HW uses a LSM6DSM sensor.  There is no existing driving for it in Zephyr, however, the LSM6DSL sensor does. I looked at the differences between the 2 devices and it comes down to the LSM6DSM having 2 extra connection modes (Modes 3 &...

jkullds by Associate II
  • 1200 Views
  • 1 replies
  • 0 kudos

LIS2MDL 3-axis magnetometer to calculate Yaw

we are using LIS2MDL magnetometer calculate yaw (Angle) data. we have integrated the LIS2MDL 3-axis magnetometer along with the ISM330DHCX. However, the resulting yaw data fluctuates, even when the sensors are stationary (without motion).From our und...

ssk2024 by Associate
  • 1240 Views
  • 1 replies
  • 0 kudos