cancel
Showing results for 
Search instead for 
Did you mean: 

Quick start Rotating dice

MK..1
Senior

Hi

I have a custom pcb design with a lsm6dsv and lsm303agr. So far it is only streaming xyz coordinates.

I need to come up with something like a rotating dice in this Video at minute 5:20 :https://www.youtube.com/watch?v=1mV_L-KEMy0

In fact i need to Show the orientation of human head and not a dice.

Which Tutorial or example project do you recommend as starting point?

Is it correct that with lsm6dsv the Gyro has a good Performance, so i dont even need the magnetometer for drift correction?

Is lsm6dsv the right chip, or is a better pin compatible chip in the lsm6 family?

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @MK..1 ,

You can look at this article.

In addition, the user manual of the MotionFX could be helpful!

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Federica Bossi
ST Employee

Hi @MK..1 ,

You can look at this article.

In addition, the user manual of the MotionFX could be helpful!

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.