MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! E compass library (LSM6DSLTR + IIS2MDCTR)

Hello  I have my oven custom board in which I used accelerometer (LSM6DSLTR), magnetometer (IIS2MDCTR) and STM32L4 series controller. Initially I tried to get north heading through magnetometer but due to external noise some time I am getting proper ...

Reset SFLP on LSM6DSV16?

HI,Is there any way to reset SFLP "Game vector" readings at runtime, once SFLP enabled?For instance, after few minutes of SFLP run, it reports (after quaternion to Euler conversion) YAW: 1.5, PITCH: 0.5, ROLL: 0.1. And I'd like to reset Yaw to 0 (zer...

bear2023R by Associate III
  • 1679 Views
  • 1 replies
  • 1 kudos

ASM330LHHXG1 does not take the DRDY flag to high

I am trying to get data from ASM330LLHXG1 so first, I decided to try the self test code provided by ST to see whether I can make the sensor work, until the reading of status register it was going okay but no matter how long I wait the status register...

eds by Associate III
  • 1190 Views
  • 1 replies
  • 0 kudos

Free Fall and Blue SDK

Hi. I'm currently working with the Blue SDK and trying to detect any falls from the SensorTile.Box Pro. The device is able to detect falls, but I am unsure of how to send that data over to my android application. I have a modified BLESensorPnPL demo ...

NeoWei by Associate II
  • 1413 Views
  • 2 replies
  • 0 kudos

Resolved! Gyroscope L3GD20 on STM32-F411E Discovery Board

Hey,I'm trying to print the data from the gyroscope L3GD20 of the STM32-F411E Discovery board ( Board Ref:MB1115B) using stm32CubeIDE.Is there a library I can use for the gyroscope, Or does any one can guide me through creating the project as it is t...

gammmmmm by Associate II
  • 2681 Views
  • 4 replies
  • 3 kudos

IIS2MDC Magnetometer burn-in

Does the IIS2MDC require burn-in? Using the IIS2MDC, I read a magnetic filed of 0.47 Gauss on a Friday. I read the same result the Monday morning at 10 am. Two hours later, I was reading 0.4 Gauss magnitude. The individual axes were also quite differ...

VCu by Associate
  • 1011 Views
  • 0 replies
  • 0 kudos

LSM6DSV16X double tap interrupt stops triggering

Hello,I am using the LSM6DSOX IMU to detect a double tap. The IMU is connected to SPI1 of a STM32U5 and the INT1 pin is connected to a GPIO (PB2) of the STM32U5 configured as external interrupt.Sometimes the double tap detection works correctly but s...

BEnge.1 by Associate III
  • 1444 Views
  • 2 replies
  • 0 kudos

h3lis331dl trigger and data

Hi,I am using h3lis331dl accelerometer with imx8mp and also using the default st_accel and st_accel_i2c drivers in Linux. Most of the part works correctly. I am using udevadm to monitor the trigger in C# code./bin/udevadm monitor iio:device0This work...

CHRISTOA by Associate
  • 1511 Views
  • 2 replies
  • 0 kudos