2024-09-25 11:33 PM - edited 2024-09-25 11:51 PM
The filter link of asm330 gyroscope includes LPF1 and LPF2, in which LPF1 can be configured with bandwidth, and LP2 is related to ODR. May I ask how much phase shift is corresponding to each filter in different bandwidth or configuration mode? Or could you provide the transfer function of the gyroscope? I need to analyze the frequency characteristics of the gyroscope under different configurations to meet the requirements of the system I designed, thank you!
2024-11-08 7:10 AM