MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STEVAL-MKI231KA (STHS34PF80) wakeup

Hello I I'm using the -> GitHub - STMicroelectronics/STMems_Standard_C_drivers, for presence and motion detect with a NUCLEO-F401RE directly connected with STEVAL-MKI231KA, i can read the sensor ID and setup the other paramethers, but my question is ...

PCabr.1 by Associate II
  • 856 Views
  • 1 replies
  • 0 kudos

Resolved! LIS2DW12 no access to registers

Hello, I am using STM32H745 to setup and communicate with LIS2DW12 accelerometer via SPI 4-wires. I am trying to setup the accelerometer and I started with reading the WHO_AM_I register. It's default value is (43h) and I changed the value of the firs...

image.png Capture d'écran 2024-07-19 142744.png
NuEta by Associate
  • 1241 Views
  • 3 replies
  • 0 kudos

LSM6DSO tilt function no working.

Hi, i'm trying to enable the tilt feature in an LSM6DSO on INT1 or INT2 but isn´t been possible until now. I´ve read the datasheet and used the example as template but for some reason the interrupt is not working. Looks like the embedded functions ar...

Resolved! MPL115A2 withSTM32 NUCLEO-H723ZG

Hello! I didn't find Driver of MPL115A2 for STM32, I tried to create a simple oneI'm not able to get dynamic data from the sensor.I connected it as below:VDD > STM32 3.3VGND > STM32 GNDSCL > PB8SDA > PB9HSR > not connectedSDWN > not connectedThis is ...

clarification regarding sensor orientation

Hi everyone!!!i am working on motionEC library and there i have observed that it need sensor orientation. can anyone explain me what exactly is this orientation meaning and how it effects the library??reagards,regards,ANIL.

Anil3 by Associate III
  • 522 Views
  • 1 replies
  • 0 kudos

LIS2DUX12

I DEVELOP A  STEP COUNTER USING lis2dux12 CHIP.I WANT TO KNOW I HOW I SETUP INTERRUPT IN STEP COUNTER

S1 by Associate II
  • 764 Views
  • 1 replies
  • 0 kudos