MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DUX12

I DEVELOP A  STEP COUNTER USING lis2dux12 CHIP.I WANT TO KNOW I HOW I SETUP INTERRUPT IN STEP COUNTER

S1 by Associate II
  • 764 Views
  • 1 replies
  • 0 kudos

LIS3MDL Temperature problem.

Hello. We know that lis3mdl is temperature sensitive, i.e. there is a scale shift. From what we have read, this cannot be compensated for with software ( Or maybe it's possible? ). Therefore, can this be prevented physically, e.g. by using some therm...

TBart.1 by Associate II
  • 829 Views
  • 3 replies
  • 0 kudos

LSM6DSV16BX Angular random walk and in-run bias stability

Hi, I am considering IMUs from ST and ADI - ADIS16505. I found that ADI provide their IMUs with "in-run bias stability" and "angular random walk", but ST does not. I also checkout the community about this, and ST only test IMUs in characterization. I...

bdang by Associate
  • 622 Views
  • 1 replies
  • 0 kudos

LPS27HHTW guidelines for system integration

Hello everyone, I'm looking for an application note (similar to AN5063 but for the LPS27HHTW sensor) to get an idea of the mechanical integration and any necessary tolerances. Additionally, I wanted to ask the community if anyone has installed two se...

LuigiG by Associate
  • 641 Views
  • 1 replies
  • 2 kudos

LIS2D12

I use LIS2DS12 This is my init function   void LIS2DS12_Init(void) { uint8_t ctrl_1 = 0x72; //0111 for 6.4kHz ODR [7:4], 00 for 2g [3:2], 1 for high frequency available[1], 0 for BDU not activated [0] uint8_t ctrl_2; // [6] for soft_reset, [1] for ...

fru999_0-1719563774185.png fru999_1-1719563790647.png
fru999 by Associate III
  • 4090 Views
  • 27 replies
  • 3 kudos

Resolved! Common SPI - LPS22HB pressure/temp sensor

Dear ST technical support.Please can you advise the pin configuration and bus timing (period between active devices) to allow me to connect three of your LPS22HB pressure sensors in parallel on the same SPI bus?The CS pin is used to enable the SPI fu...

DuncanR by Associate II
  • 2105 Views
  • 6 replies
  • 1 kudos

LIS3MDL: unexpected readings

Posted on June 05, 2017 at 20:31Hi,We're using LIS3MDL to detect changes in the earth magnetic field due to various metallic objects flowing in the sensor proximity. So, we are not interested in the correctness of the absolute values in order to pro...