MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DH - suspected noise

Posted on July 02, 2015 at 14:53Hello there, I had placed the LIS2DH on my board , and it seems to work fine. using default setting and 10Hz sampling, when i am putting the PCBA on a fixed position, and X axis raw data is unstable from - 128 to 128....

nir23 by Associate
  • 702 Views
  • 0 replies
  • 0 kudos

Unable to get axis data on LIS2DHH

Posted on July 02, 2015 at 14:50Hey, I have to communicate with LIS2DHH , and dummy byte received fine, however when i am trying to read axis data i get only 0.

nir23 by Associate
  • 760 Views
  • 0 replies
  • 0 kudos

Did I just brick my evaluation board?

Posted on December 17, 2013 at 16:12Hello,I bought a STEVAL-MKI109v1  evaluation board, and a STEVAL-MKI114v1 probe about 1,5 years ago.Yesterday I tried to get it to work with the latest version of the Unico test software, but the program would alw...

joeri by Associate
  • 1665 Views
  • 2 replies
  • 0 kudos

Capacitance/Voltage Converter

Posted on June 24, 2015 at 19:36Hello all, I would like to use an off-the-shell CVC as readout for my capacitive MEMS accelerometer. My concern is the acceptable input bulk capacitance, that is 30pF in my case. I have looked in a couple of CVCs, MS...

AHRS continous problem under CoIDE

Posted on April 19, 2015 at 20:33 Hi to all, I'm trying to use this demo, and I have noticed that my program remains blocked at this line of the iNEMO_AHRS_Init() void iNEMO_AHRS_Init(iNEMO_SENSORDATA* pSensorData, iNEMO_EULER_ANGLES* pAngle,...

daniel23 by Associate II
  • 1286 Views
  • 2 replies
  • 0 kudos

A terrible question when i use MP45DT02

Posted on August 16, 2014 at 06:03Hi,I am Jessenow,i will use MP45DT02 in my projectbut i evaluated it in STM32F407-DISCOVERY,i found a kind of terrible noise , it sounds like ''dot……dot……dot……'',especially female voice.wish a solutionthank you very...

LIS3DSH noise problem

Posted on June 09, 2015 at 15:36Hi,I am using LIS3DSH accelerometer, sampling rate 100HZ scale = +-2G. What I see is from time to time is noise what is coming from one of the axis, I tried to add more decoupling caps, thy to change internal filter s...

LSM303D Magnetic Offset Registers

Posted on June 03, 2015 at 17:02 While working with the LSM303D, I ran into the following problem: The application:To detect disturbances in the local magnetic field (the sensor is stationary). I average a set of readings, and then su...

Nucleo-L053R8 with SHT15 humidity& temp sensor.

Posted on May 21, 2015 at 16:09Hi,I'm using SHT15 to measure temp&humidity. Here,I connected I2C1_SCL  in PB6.I2C1_SDA in PB7.I attached the SHT drivers i created. Unfortunately, I couldn't see the values on serial communication. Could some one look...

gandhi by Associate II
  • 962 Views
  • 1 replies
  • 0 kudos