User Activity

Posted on June 21, 2016 at 16:28Hi,I'm using STM32L053R8 for my data logger project. I would like to see lutra low powers. My custom board which is running by MSI clock is consuming 2.2mA. I'm running with only MSI clock i.e.2MHZ. In the attached im...
Posted on April 20, 2016 at 14:06Hi,I'm new bee here. My project needs to consume very less power. I see that STM32L053R8 consumes 88µA/MHZ that means it takes 88µA*16 for 16MHZ? or is it different?. I would like to perate my controller at 5MHZ only...
Posted on January 06, 2016 at 11:46Hi, I'm developing a data logger using STM32L053R8. I'm preparing the custom board with some sensors. I would like to use a On/Off button to my board. I wondering to which pins and how can i implement this hardware...
Posted on December 21, 2015 at 15:50Hi,I'm a software dveloper working in Germany. Our company is planning to develop a data logger product with temp,humidity,3-axis and light sensors also with a serial flash memory.I'm working on nucleo-L053R8 boar...
Posted on November 03, 2015 at 10:27Hi,I'm planning to get 3200Hz data rates for ADXL345 sensor with Nucleo board. The SPI speed is 5MHz. And i initialized exactly as per the data sheet.the initialization process is as below:accelerometer.setPowerCo...