MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Data Ready Interrupt H3LIS331DL

Posted on February 04, 2014 at 08:30How does one configure the data ready interrupt on the H3LIS331DL accelerometer? I've configured other accelerometers like LIS3DSH with success but I am stuck on this one.I've tried both latched and pulsed interru...

dmg0048 by Associate II
  • 2014 Views
  • 3 replies
  • 0 kudos

lsm6ds3 drivers

Posted on December 12, 2016 at 14:54Can somebody share linux device drivers for kernel 3.7.6 drivers for lsm6ds3

lps22hb no pressure and temperature response

Posted on December 11, 2016 at 07:25I have connected LPS22HB development kit (STEVAL-MET001V1) and Raspberry Pi 3 with I2C interface and tried to read pressure and temperature data but whatever setting I tried, pressure (0x28, 0x29, 0x2A) and temper...

Free-fall and motion detection simultaneously on LIS3DH

Posted on November 29, 2016 at 23:46Hi support,We wonder if there is any register configuration that allow us to route the motion detection to the INT1 pin and the free-fall detection to the INT2 pin and both working at the same time? Both pins are ...

jgaldana by Associate II
  • 1027 Views
  • 1 replies
  • 0 kudos

LIS3DHTR data length

Posted on November 02, 2016 at 07:41What is the actual data (x,y,z) length. When I'm reading the acceleration data , the lowest 4 bitsare 0. This would indicate the data is actually 12bit , left justified. The datasheet however say's the FIFO is 10b...

Rob1 by Associate II
  • 1477 Views
  • 2 replies
  • 0 kudos

X-CUBE-MEMSMIC : Extension to 6 microphones

Posted on January 12, 2016 at 15:18Hello, I need help with regard to extending the 4 microphone architecture of X-CUBE-MEMSMIC to 6 microphones using X-NUCLEO-CCA02M1 and STEVAL-MKI155V3. I have attached the modified BSP driver .c and .h files. Also...

MP23DB01MM datasheet

Posted on September 07, 2016 at 10:40Hello,I saw that MP23DB01MM is used in BlueCoin  device. I would like to investigate this microphones characteristics but  could not find a data sheet. Please could you redirect me to data sheet web page ?Thanks ...