MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

what is the exact principle of time of flight technology?

Posted on December 17, 2016 at 06:48Hi, i searched for the exact principle of the time of flight technology in internet but the answer i got was different in different websites. I bought VL53l0X sensor recently and i need the exact principle of TOF ...

Resolved! IIS2DH interrupt generation and tech details

Posted on November 04, 2016 at 15:57Hi,I would like to use IIS2DH accelerometer as main accelerometer in a custom board for my project. For this reason I've bought the STEVAL-MK1168V1 to make some tests. I would like to ask you some questions about ...

Why is there no self-test function of the magnetometer in LSM303D?

Posted on December 15, 2016 at 10:23Hi there,   According to the datasheet of LSM303D, I could find the self-test function of the accelerometer, but could not find the same function of the magnetometer.   How to test the magnetometer if no build-in ...

looeyc by Associate II
  • 927 Views
  • 1 replies
  • 0 kudos

Resolved! Test LSM6DS3 interrupt with Self Test

Posted on December 15, 2016 at 16:25Hi Everybody, I want to test the interrupt of the LSM6DS3 sensor without any movement. Do you know if it is possible to generate an interrupt with the sensor self test ?If I program a low interrupt threshold and I...

Jerome V by Associate II
  • 2213 Views
  • 5 replies
  • 0 kudos

Resolved! schizophrenic LIS3DS0

Posted on November 28, 2016 at 17:59Hi everybody,We are using LIS3DS0 on the ISK01A1 board monted on a Nucleo F103-RB...Our software is based on HAL drivers (got in the cube).We met this strange issue in some of our boards (we confirmed the test wit...

samuel23 by Associate III
  • 2234 Views
  • 6 replies
  • 0 kudos

SPI COMMUNICATION NOT WORKING

Posted on November 02, 2016 at 23:14Hello Everyone,I am having trouble talking to the LSM6DS3 using 4 wire SPI. I have verified the signals to the device as being correct per the datasheet. I am commanding 0x8F to do a WHO_AM_I command but am not se...

kyle2 by Associate
  • 1901 Views
  • 3 replies
  • 0 kudos

LSM6DS3 interrupt pin not going back to low state

Posted on August 10, 2016 at 06:08I brought STEVAL-MKI160V1 MEMS sensor board. Bulk ID Z5T42380E024. While working with the sensor I got an issue like I enabled interrupt generation to interrupt pin INT1 for 6D orientation detection. So when ever I ...

n239955 by Associate
  • 1122 Views
  • 1 replies
  • 0 kudos

About LSM330 Register Problem

Posted on February 26, 2014 at 03:15Currently, I am now using LSM330, the only reference driver I found is official Linux-OS driver. Since there's no programming guides, I search website for source code for reference, only to find that all source co...

leo2010 by Associate
  • 806 Views
  • 1 replies
  • 0 kudos

Data Ready Interrupt H3LIS331DL

Posted on February 04, 2014 at 08:30How does one configure the data ready interrupt on the H3LIS331DL accelerometer? I've configured other accelerometers like LIS3DSH with success but I am stuck on this one.I've tried both latched and pulsed interru...

dmg0048 by Associate II
  • 1993 Views
  • 3 replies
  • 0 kudos

lsm6ds3 drivers

Posted on December 12, 2016 at 14:54Can somebody share linux device drivers for kernel 3.7.6 drivers for lsm6ds3