MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FIFO alignment is not correct after some time

Posted on September 26, 2016 at 23:15We enabled GyroScope and acclerometer. We set FIFO Mode to continuous with BDU bit is set. We set ODR rate to 1.66kHz . We are reading FIFO continuously. we are observing FIFO data mis-alignment Can somebody help...

Unexpected current consumption from LSM303D

Posted on February 04, 2017 at 03:36Hi,   We are developing a ultra low power sensor module with the LSM303D. The LSM303D was periodically waken up to take a  magnetic and temperature measure (no acceleration measurment). The total excepted average ...

0690X00000603MmQAI.jpg
looeyc by Associate II
  • 621 Views
  • 1 replies
  • 0 kudos

LSM9DS0 Accelerometer noise

Posted on January 17, 2017 at 19:16Hi.I am using the LSM9DS0, and have observed a lot of noise on the z-Axis of the Accelerometer Data. The attached picture is a plot showing the noise while operating at 100Hz in the +-2g range. Is this a normal lev...

0690X000006064IQAQ.png

LSM303D // Compass X,Y & Z's MSB locked

Posted on March 26, 2015 at 14:53 Hey there, I recently installed a new LSM303D (accelerometer + compass) on my board and I am having some issues with it. I can read the data from the accelerometer fine, but the ones from the compass seem...

STEVAL WESU1 understanding logged data

Posted on October 26, 2016 at 16:43Hi , I have STEVAL WESU module  and logged acelerometer data using android app. (plz see attached file)My settings are: Timer: 512 Hz, 10Hz, 1HzMEMS Accelerometer output data rate: 416 Hz , 833 Hz, 100HzIn the logg...

abhi1new by Associate
  • 922 Views
  • 2 replies
  • 0 kudos

Reading status register of LSM6DS3

Posted on January 31, 2017 at 06:12hi,     I am Reading the Accelerometer and Gyroscope sensor values by checking the XLDA and GDA bits as follows             if((readReg(STATUS_REG)&0x01)==0x01)     // checking XLDA        {              Ax = (int1...

Problem reading value gyroscope

Posted on January 27, 2017 at 15:04Hello, sorry for me level in EnglishI have to carry out an end of year project of electronic bts, and I am stuck at this levelI need your help to understand a lack of reading in the following code I use this soft :...

How compatible are LSM6DSL and LSM6DS3?

Posted on January 27, 2017 at 00:19We were looking at using the LSM6DS3 in a new design, but I noticed the LSM6DSL uses half the power.  The two parts look to be pin compatible and probably software compatible (at least for most features).  Is that ...